ArcGIS Login Providers

The ArcGIS Login Providers subtab deals with the configuration of your portal. This is an extremely technical view of your Auth Model. After the initial setup, it’s likely you would only change a few items, such as Client Secret and URL.

IMPORTANT: If you need a new portal, reach out to ArcFMReadiness@se.com for assistance.

The new Auth Model displays in the list on the left of the Solution Center window.

You can make changes to an existing Auth Model as needed. Select the Auth Model you want to change from the list on the left, and update the fields on the right (for example, the Client Secret and URL fields).

The User Profile Script uses .json validates as you type. Before making changes, copy and paste the existing script in another application as a backup.

If you save incorrect edits, then you won’t be able to log in to your tenant any more. If this happens to you, reach out to ArcFMReadiness@se.com for assistance. Solution Center creates nightly backups of this data and likely can retrieve your configuration prior to any recent changes you made.


Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.