Markup Settings

The credentials are used for machine-to-machine (M2M) communications when markup is trying to communicate with ArcGIS Server to send and receive markups.

IMPORTANT: Create a Portal account for these M2M communications. Additionally:
  • The Portal account can be the same for Sync Settings and Markup Settings. Or, for more granular access control, use a separate Portal account for Markup Settings and Sync Settings.

  • For Markup Settings, the Portal account must have access to all Markup feature services.

NOTE: As discussed in the Cybersecurity Best Practices topic in the ArcFM XI Series Architecture Guide, Schneider Electric strongly recommends regularly cycling the M2M credentials.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.