Earth-Leakage Protection
Presentation
Earth-leakage protection on MicroLogic 7 trip units provides protection against low intensity fault currents to ground for:
-
All types of electrical distribution applications
-
People, according to the earth-leakage protection setting used
Earth-leakage protection is designed for installations with TT or TN-S grounding system.
The MicroLogic 7 electronic trip unit is available in two versions for earth-leakage detection:
-
The Trip version trips when earth-leakage is detected.
-
The Alarm version measures the earth-leakage current and indicates an earth-leakage fault on the display screen.
Operating Principle
Earth-leakage protection is definite time.
The earth-leakage protection threshold IΔn sets the level of earth-leakage current at which the circuit breaker trips when reaching the earth-leakage protection time delay Δt.
Setting the Earth-Leakage Protection
Set the IΔn pickup with the MicroLogic 7 trip unit IΔn dial.
Set the Δt time delay as follows:
-
With the keypad on the MicroLogic 7 trip unit
-
With EcoStruxure Power Commission software (password-protected)
IΔn Pickup Setting Values
|
Trip unit rating In (A) |
Pickup IΔn |
||||||||
|---|---|---|---|---|---|---|---|---|---|
|
IΔn dial position |
1 |
2 |
3 |
4 |
5 |
6 |
7 |
8 |
9 |
|
40, 100, 160, and 250 A |
30 mA |
30 mA |
100 mA |
300 mA |
500 mA |
1 A |
3 A |
5 A |
OFF |
|
400 and 570 A (1) |
300 mA |
300 mA |
500 mA |
1 A |
3 A |
5 A |
10 A |
10 A |
OFF |
|
(1) Maximum setting at 570 A for thermal reasons, to be adapted with breaking block up to 630 A |
|||||||||
The accuracy range is +/-10%.
Δt Time Delay Setting Values
When IΔn is set to the 30 mA, the earth-leakage protection acts immediately (instantaneous tripping), whatever the setting of the Δt time delay.
For other IΔn values (> 30 mA), the Δt time delay can be set to one of the following values:
-
0 s
-
60 ms
-
150 ms
-
500 ms
-
1 second
Testing the Earth-Leakage Protection (With Trip) Using Test Button
On the Trip version of MicroLogic 7 trip units, the earth-leakage protection must be tested regularly by using the test button T. Pressing the test button simulates a real leakage current passing through the toroid and the circuit breaker trips.
When the earth-leakage protection pickup IΔn is set to the OFF position, pressing the test button has no effect.
The earth-leakage function test can be
performed with the padlock locked
or unlocked
.
Follow these steps to test and reset the earth-leakage protection on MicroLogic 7 trip units:
|
Step |
Action |
Display |
|---|---|---|
|
1 |
Energize the circuit breaker. |
– |
|
2 |
Open the protective cover of the trip unit. |
– |
|
3 |
Provide a power supply to the trip unit so that the screen displays the result of the test after the circuit breaker trips. |
– |
|
4 |
Push the toggle handle from the position to the position. The circuit breaker is closed. |
|
|
5 |
Press the test button T: the circuit breaker trips. is displayed on the screen for two seconds and then the screen displays 0 A. NOTE: If the circuit breaker does not trip, the earth-leakage protection
is no longer active. Analyze the cause and replace the MicroLogic 7 trip unit or the circuit breaker.
|
|
|
6 |
Push the toggle handle from the (Trip) position to the position. |
|
|
7 |
Push the toggle handle from the position to the position. The circuit breaker is closed. |
Testing the Earth-Leakage Alarm (Without Trip) Using Test Button
On the Alarm version of the MicroLogic 7 trip unit, the earth-leakage alarm can be tested by using the test button T. Pressing the test button simulates a real leakage current passing through the toroid. The circuit breaker does not trip.
When the earth-leakage alarm pickup IΔn is set to the OFF position, pressing the test button has no effect.
The earth-leakage function test can be performed with the padlock
locked
or unlocked
.
Follow these steps to test the earth-leakage alarm on MicroLogic 7AL trip units:
|
Step |
Action |
Display |
|---|---|---|
|
1 |
Energize the circuit breaker. |
– |
|
2 |
Open the protective cover of the trip unit. |
– |
|
3 |
Provide a power supply to the trip unit. |
– |
|
4 |
Push the toggle handle from the position to the position. The circuit breaker is closed. |
|
|
5 |
Press the test button T: is displayed on the screen for two seconds, and then the previous screen is displayed. NOTE: If is displayed on the screen,
the earth-leakage alarm is no longer active. Replace the MicroLogic 7AL trip unit.
|
Testing the Earth-Leakage Function (Without Trip) Using Keypad Only
On the Trip and Alarm versions of the MicroLogic 7 trip unit, the earth-leakage tripping chain (or earth-leakage detection for the Alarm version) (except mechanism and pole operation) can be tested, without tripping the circuit breaker, by using the keypad.
The earth-leakage function test can be
performed with the padlock locked
or unlocked
.
Follow these steps to test the earth-leakage protection alarm on MicroLogic 7AL trip units:
|
Step |
Action |
Using |
Display |
|---|---|---|---|
|
1 |
Select the earth-leakage measurement screen. |
||
|
2 |
Access the earth-leakage function test by pressing . The pictogram appears and the pictogram blinks. |
||
|
3 |
Prompt the earth-leakage function test by pressing . The result of the test ( or ) is displayed on the screen after two seconds. NOTE: If is displayed
on the screen, test the earth-leakage function by using the test button .
|
||
|
4 |
After two seconds the screen returns to the screen displayed before the test |
– |
– |
Earth-Leakage Test History
The last ten earth-leakage tests are recorded in an earth-leakage test history. Tests performed using the T test button and tests using the keypad are logged in the same history.
The history records:
-
Type of test: with trip or without trip
-
Date of test
-
Result of test ( or )
The earth-leakage test history can be consulted:
-
With EcoStruxure Power Commission software.
-
On a remote controller using the communication network.
Resetting the Circuit Breaker After an Earth-Leakage Fault Detection
Resetting the earth-leakage function after an earth-leakage fault detection (with or without trip) depends on the version:
-
For the Trip version, reset the circuit breaker by moving the handle from to position, and then to position. Acknowledge the earth-leakage trip screen by pressing .
-
For the Alarm version, acknowledge the earth-leakage trip screen by pressing .
Resetting the earth-leakage function after an earth-leakage protection test is described in the procedure for each test.