Long-Time Protection
Presentation
Long-time protection on MicroLogic 6 E-M trip units protects all types of motor applications against overload currents.
Operating Principle
Long-time protection is I2t IDMT (Inverse Definite Minimum Time):
-
It incorporates the motor thermal image function.
-
It can be configured as the Ir pickup and as the trip class Class.
Tripping curve:
|
The long-time protection parameters are:
|
Setting the Long-Time Protection
Set the Ir pickup:
-
With the MicroLogic trip unit Ir dial to preset the value and the keypad to fine-tune the value
-
With EcoStruxure Power Commission software (password-protected)
-
By sending a setting command using the communication network (password-protected)
Set the trip class Cl:
-
With the keypad on the MicroLogic trip unit
-
With EcoStruxure Power Commission software (password-protected)
-
By sending a setting command using the communication network (password-protected)
Ir Pickup Setting Value
The default Ir pickup setting value is In (maximum dial value).
The overload or thermal protection tripping range is 1.05–1.20 x Ir according to standard IEC/EN 60947-2.
The Ir pickup is preset by a dial.
|
In Rating |
Preset values of Ir (A) depending on the trip unit In rating and the dial position |
||||||||
|---|---|---|---|---|---|---|---|---|---|
|
25 A |
12 |
14 |
16 |
18 |
20 |
22 |
23 |
24 |
25 |
|
50 A |
25 |
30 |
32 |
36 |
40 |
42 |
46 |
47 |
50 |
|
80 A |
35 |
42 |
47 |
52 |
57 |
60 |
63 |
72 |
80 |
|
150 A |
70 |
80 |
90 |
100 |
110 |
120 |
133 |
140 |
150 |
|
220 A |
100 |
120 |
140 |
155 |
170 |
185 |
200 |
210 |
220 |
|
320 A |
160 |
180 |
200 |
220 |
240 |
260 |
280 |
300 |
320 |
|
500 A |
250 |
280 |
320 |
360 |
380 |
400 |
440 |
470 |
500 |
The accuracy range is + 5%/+ 20%.
Use the keypad to fine-tune the setting, in increments of 1 A:
-
The setting range maximum is the preset value displayed by the dial.
-
The setting range minimum is the minimum preset value.
Example:
A MicroLogic 6 E-M trip unit In = 500 A is preset by the dial at 470 A. The fine-tuning range on the keypad is 250–470 A.
Trip Class Setting Value
The class is set via the keypad, using any of the four defined values: 5, 10, 20, and 30.
The trip class corresponds to the value of the trip time delay for a current of 7.2 x Ir according to standard IEC/EN 60947-4-1.
The factory class setting value is 5 (minimum value).
The following table shows the value of the trip time delay depending on the current in the load for all four trip classes.
|
Current in the load |
Trip class Cl |
|||
|---|---|---|---|---|
|
5 |
10 |
20 |
30 |
|
|
tr Trip time delay (s) |
||||
|
1.5 x Ir |
120 |
240 |
400 |
720 |
|
6 x Ir |
6.5 |
13.5 |
26 |
38 |
|
7.2 x Ir |
5 |
10 |
20 |
30 |
Motor Thermal Image
The model representing heat rise and cooling in a motor load is identical to that used for the conductors. It is constructed according to the algorithm for calculating the thermal demand but this model takes account of the iron and copper losses.
Thermal Memory
MicroLogic 6 E-M trip units incorporate a thermal memory which ensures that the conductors are cooled even after tripping: cooling lasts for 20 minutes before or after tripping.
Cooling Fan
By default, the motor thermal image is calculated taking account of the fact that the motor is self-cooled (fan mounted on the shaft end).
If the motor is force-cooled (forced ventilation), the calculation of the thermal image takes account of the shortest time constants for the cooling calculation.
The cooling ventilation parameters (Auto or Moto position) are set on the MicroLogic trip unit keypad or using EcoStruxure Power Commission software.