DOCA0188EN-03

Instantaneous Protection

Presentation

Instantaneous protection on MicroLogic 6 E-M trip units protects all types of motor applications against very high intensity short-circuit currents.

Operating Principle

Instantaneous protection is fixed: the pickup value is determined by the trip unit rating. Protection is instantaneous.

Tripping curve:

The instantaneous protection parameters are:

  • A: In Trip-unit setting range

  • F: Ii Instantaneous protection pick-up

Ii Pickup Value

The Ii pickup value is directly determined by the trip unit In rating and is in x In.

Ii pickup value according to the MicroLogic trip unit In rating (accuracy range +/-10%).

In rating (A)

25

50

80

150

220

320

500

Instantaneous pickup (A)

425

750

1200

2250

3300

4800

7500

The hold time is 0 ms.

The maximum breaking time is 30 ms.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?