Ground-Fault Protection
Presentation
Ground-fault protection on MicroLogic 6 E-M trip units protects all types of motor applications against ground-fault currents in the TN-S system. For more details, refer to DOCA0187•• ComPacT NSX - Circuit Breakers and Switch-Disconnectors 100–630 A - User Guide.
Operating Principle
Ground-fault protection is definite time. It can be configured as Ig pickup and as tg trip time delay.
Tripping curve:
Setting the Ground-Fault Protection
Set the Ig pickup:
-
With the MicroLogic trip unit Ig dial to preset the value and the keypad to fine-tune the value
-
With EcoStruxure Power Commission software (password-protected)
-
By sending a setting command using the communication network (password-protected)
Set the tg time delay:
-
With the keypad on the MicroLogic trip unit
-
With EcoStruxure Power Commission software (password-protected)
-
By sending a setting command using the communication network (password-protected)
Ig Pickup Setting Values
The Ig pickup setting value is in multiples of In.
The default Ig pickup setting value is the same as the minimum dial value:
-
0.60 In for trip units rated 25 A
-
0.30 In for trip units rated 50 A
-
0.20 In for trip units rated > 50 A
Ground-fault protection can be deactivated by setting the Ig dial to the OFF position.
Ground-fault protection can be reactivated even with the Ig dial in the OFF position:
-
By fine-tuning on the keypad
-
With EcoStruxure Power Commission software (password-protected)
-
By sending a setting command using the communication network (password-protected)
The following three tables specify the setting values (preset by a dial) and setting ranges (set on the keypad):
-
For trip units rated 25 A
-
For trip units rated 50 A
-
For trip units rated > 50 A
On the keypad, the increment is 0.05 x In.
Rating 25 A
|
Type of setting |
Value or setting range (x In) |
||||||||
|---|---|---|---|---|---|---|---|---|---|
|
Preset by a dial |
0.60 |
0.60 |
0.60 |
0.60 |
0.70 |
0.80 |
0.90 |
1 |
OFF |
|
Setting range on the keypad |
0.60 |
0.60 |
0.60 |
0.60 |
0.6–0.7 |
0.6–0.8 |
0.6–0.9 |
0.6–1 |
0.6–1 + OFF |
Rating 50 A
|
Type of setting |
Value or setting range (x In) |
||||||||
|---|---|---|---|---|---|---|---|---|---|
|
Preset by a dial |
0.30 |
0.40 |
0.50 |
0.60 |
0.70 |
0.80 |
0.90 |
1 |
OFF |
|
Setting range on the keypad |
0.30 |
0.3–0.4 |
0.3–0.5 |
0.3–0.6 |
0.3–0.7 |
0.3–0.8 |
0.3–0.9 |
0.3–1 |
0.3–1 + OFF |
Rating > 50 A
|
Type of setting |
Value or setting range (x In) |
||||||||
|---|---|---|---|---|---|---|---|---|---|
|
Preset by a dial |
0.20 |
0.30 |
0.40 |
0.50 |
0.60 |
0.70 |
0.80 |
1 |
OFF |
|
Setting range on the keypad |
0.20 |
0.2–0.3 |
0.2–0.4 |
0.2–0.5 |
0.2–0.6 |
0.2–0.7 |
0.2–0.8 |
0.2–1 |
0.2–1 + OFF |
The accuracy range is +/-10%.
tg Time Delay Setting Values
The tg time delay setting value is in seconds. The hold and breaking times are in milliseconds.
The default tg time delay setting is 0 s.
The following table shows tg setting values in second (s) and the associated hold and breaking times in milliseconds (ms):
|
Function |
Value |
||||
|---|---|---|---|---|---|
|
tg (s) |
0 |
0.1 |
0.2 |
0.3 |
0.4 |
|
Hold time (ms) |
20 |
80 |
140 |
230 |
350 |
|
Maximum breaking time (ms) |
80 |
140 |
200 |
320 |
500 |
Testing the Ground-Fault Protection
The ground-fault protection can be tested to check the electronic tripping function of the trip unit. Use the keypad of the MicroLogic 6 trip unit to perform this test.
The ground-fault protection test can be performed with the padlock
locked
or unlocked
.
Follow these steps to test and reset the ground-fault protection on MicroLogic 6 trip units.
|
Step |
Action |
Display |
|---|---|---|
|
1 |
Provide a power supply to the trip unit so that the screen displays the result of the test after the circuit breaker trips. |
– |
|
2 |
Select the Instantaneous measurement readout mode (the display is the most heavily loaded phase, in this example Phase 2). |
|
|
3 |
Select the ground-fault current measurement screen (the value is a percentage of the Ig setting). |
|
|
4 |
Access the ground-fault protection test function by pressing . The pictogram appears and the pictogram blinks. |
|
|
5 |
Prompt the ground-fault protection test by pressing . The circuit breaker trips. The ground-fault protection trip screen is displayed. |
|
|
6 |
Acknowledge the ground-fault trip screen by pressing . The pictogram blinks. |
|
|
7 |
Confirm by pressing again. The confirmation is displayed for 2 s. |