Harmonic Currents
Origin and Effects of Harmonics
Many nonlinear loads present on an electrical network creates a high level of harmonic currents in the electrical networks.
These harmonic currents:
-
Distort the current and voltage waves
-
Degrade the quality of the distributed energy
These distortions, if they are significant, can result in:
-
Malfunctions or degraded operation in the powered devices
-
Unwanted heat rises in the devices and conductors
-
Excessive power consumption
These various problems increase the system installation and operating costs. It is therefore necessary to control the energy quality carefully.
Definition of a Harmonic
A periodic signal is a superimposition of:
-
The original sinusoidal signal at the fundamental frequency (for example, 50 Hz or 60 Hz)
-
Sinusoidal signals whose frequencies are multiples of the fundamental frequency called harmonics
-
Any DC component
This periodic signal is broken down into a sum of terms: 
where:
-
y0: Value of the DC component
-
yn: rms value of the nth harmonic
-
ω: Pulsing of the fundamental frequency
-
ϕn: Phase displacement of harmonic component n
RMS Currents and Voltages
MicroLogic trip units display the rms values of currents and voltages.
Acceptable Harmonic Levels
Various standards and statutory regulations set the acceptable harmonic levels:
-
Electromagnetic compatibility standard adapted to low voltage public networks: IEC/EN 61000‑2‑2
-
Electromagnetic compatibility standards:
-
For loads below 16 A: IEC/EN 61000-3-2
-
For loads higher than 16 A: IEC/EN 61000-3-4
-
-
Recommendations from energy distribution companies applicable to the installations
The results of international studies have identified typical harmonic values that should not be exceeded.
The following table lists the typical harmonic values for voltage as a percentage of the fundamental:
|
Odd harmonics that are not multiples of 3 |
Odd harmonics that are multiples of 3 |
Even harmonics |
|||
|---|---|---|---|---|---|
|
Order (n) |
Value as a % of V1 |
Order (n) |
Value as a % of V1 |
Order (n) |
Value as a % of V1 |
|
5 |
6% |
3 |
5% |
2 |
2% |
|
7 |
5% |
9 |
1.5% |
4 |
1% |
|
11 |
3.5% |
15 |
0.3% |
6 |
0.5% |
|
13 |
3% |
>15 |
0.2% |
8 |
0.5% |
|
17 |
2% |
– |
– |
10 |
0.5% |
|
>19 |
1.5% |
– |
– |
>10 |
0.2% |