Readout Mode
Measurement Readout
MicroLogic 5 and 6 trip units and MicroLogic 7 trip units with integrated earth-leakage protection have the same five navigation keys. The appearance of the keys differs, as shown in the following table:
The following examples use the keys of the MicroLogic 5 and 6 trip units to illustrate navigation for readout and setting modes. For MicroLogic Vigi 7 trip units, navigation is made in the same way.
Example of Measurement Readout
The following table gives the readout values of the 3 phase currents, the phase-to-phase voltage V12, and the total active power (Ptot):
|
Step |
Action |
Using |
Display |
|---|---|---|---|
|
1 |
Select the Instantaneous measurement readout mode (the most heavily loaded phase is displayed). Read the value of current I2. |
||
|
2 |
Select the next current measurement: current I3. Read the value of current I3. |
||
|
3 |
Select the next current measurement: current I1. Read the value of current I1. |
||
|
4 |
Select the phase-to-phase voltage V12 measurement. Read the value of voltage V12. |
||
|
5 |
Select the Ptot power measurement. Read the Ptot active power. |
Energy Meter Readout
Energy meters change measurement unit automatically:
-
For active energy, Ep, displayed in kWh from 0 to 9999 kWh then in MWh
-
For reactive energy, Eq, displayed in kVARh from 0 to 9999 kVARh then in MVARh
-
For apparent energy, Es, displayed in kVAh from 0 to 9999 kVAh then in MVAh
When energies are indicated in MWh, MkVARh, or MVAh, the values display on 4 digits. The MicroLogic trip unit incorporates the option of full energy meter readout.
Reading Full Energy Values
The following table gives the full readout values of the Ep active energy meter.
|
Step |
Readout value |
Action |
Using |
Display |
|---|---|---|---|---|
|
1 |
Current in most heavily loaded phase |
Select the Readout and reset the energy meter mode (main screen displayed). |
||
|
2 |
Energy with Reset option showing |
Select the Ep active energy meter. The value displayed is (in the example), which corresponds to 10 MWh +1300 kWh (approximately). |
||
|
3 |
Specific energy measurement |
Specify the measurement. The value displayed is (in the example): the full energy meter value is 11318 kWh. |
||
|
4 |
Energy normal display |
Return to the energy meter normal display. The display reverts automatically after 5 minutes. |
Resetting Energy Meter
The energy meters can be reset with the padlock locked
or unlocked
.
|
Step |
Readout value |
Action |
Using |
Display |
|---|---|---|---|---|
|
1 |
Current in most heavily loaded phase |
Select the Measurement readout and reset energy meter mode (main screen displayed). |
||
|
2 |
Energy with Reset option showing |
Select the energy meter to be reset. |
||
|
3 |
Reset option lit |
Validate the reset. The pictogram blinks. |
||
|
4 |
OK |
Confirm the reset. The confirmation is displayed for 2 s. |
Resetting Peak Demand Values
The peak demand values can be reset with the padlock
locked
or unlocked
.
|
Step |
Readout value |
Action |
Using |
Display |
|---|---|---|---|---|
|
1 |
Main screen |
Select the Readout and reset peak demand values mode (main screen displayed). |
||
|
2 |
Peak demand with Reset option showing |
Select the peak demand to be reset. |
||
|
3 |
Reset option lit |
Validate the reset. The pictogram blinks. |
||
|
4 |
OK |
Confirm the reset. The confirmation is displayed for 2 s. |
Protection Function Readout
A protection function is selected using the
key. This selection is only
possible in Readout mode, that is, when the padlock is locked.
-
Scrolling is cyclical.
-
The up arrow indicates the selected protection function.
For the neutral protection functions, the down arrow, pointing to , replaces the up arrow.
Example of Protection Function Readout
Readout of the setting values for the long-time protection Ir pickup, tr time delay, and the short-time protection Isd pickup:
|
Step |
Readout value |
Action |
Using |
Display |
|---|---|---|---|---|
|
1 |
Long-time protection Ir pickup setting value in amperes |
Select the Protection function readout mode (main screen displayed). The long-time protection Ir pickup setting value is displayed in amps. |
||
|
2 |
Long-time protection tr time delay setting value in seconds |
Select the long-time protection tr time delay. The long-time protection tr time delay setting value is displayed in seconds. |
||
|
3 |
Short-time protection Isd pickup setting value in amperes |
Select the short-time protection Isd pickup The short-time protection Isd pickup setting value is displayed in amps. |
Neutral Status Readout (3-Pole Trip Unit)
The Neutral status readout mode is
dedicated to this function. Navigation is therefore limited to the
key.
|
Step |
Readout value |
Action |
Using |
Display |
|---|---|---|---|---|
|
1 |
Neutral status is displayed |
Select the Neutral status readout mode. The neutral status value is displayed:
|
BSCM Modbus SL/ULP Module Settings Readout (MicroLogic 5/6 Trip Units Only)
Only for MicroLogic 5 and 6 trip
units, BSCM Modbus SL/ULP module settings are read by pressing the
key for five seconds.
It is not necessary to unlock the settings with the lock/unlock microswitch to read the BSCM Modbus SL/ULP module settings.
Press the
key successively to scroll
through the setting screens.
Scrolling is cyclical.
The following BSCM Modbus SL/ULP settings can be read:
-
The Modbus address
-
The Baud rate
-
The parity