Using the ZSI Function with ComPacT NSX Circuit Breakers
Description
The MicroLogic 5 and 6 trip units support ZSI. The following figure explains how the signal wire is connected to the trip unit:

Q1 Upstream circuit breaker
Q2 Circuit breaker to be wired
Q3 Downstream circuit breaker
Z1 ZSI-OUT source
Z2 ZSI-OUT
Z3 ZSI-IN source
Z4 ZSI-IN ST short-time protection
Z5 ZSI-IN GF ground-fault protection (MicroLogic 6)
Outputs Z3, Z4, and Z5 are only available on ComPacT NSX400/630 circuit breakers.
The short-time and ground-fault protection time delay settings (MicroLogic 6) for trip units using ZSI must comply with the rules relating to selective coordination.
Connection Principles
The following figures show the options for connecting devices together:
|
Protection |
Connection diagram |
|
|---|---|---|
|
Ground-fault and short-time protection (MicroLogic 6) |
Connect output Z2 of the trip unit on the downstream circuit breaker Q2 to inputs Z4 and Z5 of the trip unit on the upstream circuit breaker Q1. |
|
|
Short-time protection |
|
|
|
Ground-fault protection (MicroLogic 6) |
|
|
Multi-Source Distribution
If a number of circuit breakers are installed upstream (as with multi-source distribution), the same principles apply.
Connect a downstream circuit breaker to all the circuit breakers installed directly upstream:
-
Connect all the commons (outputs Z1/inputs Z2) to one another.
-
Connect output Z2 simultaneously to inputs Z3, Z4, or Z5 of all the circuit breaker trip units installed upstream.
Connection Wire Characteristics
The following table indicates the characteristics of the inter-device signal wire:
|
Characteristics |
Values |
|---|---|
|
Impedance |
50 Ω per 300 m |
|
Maximum length |
300 m |
|
Type of cable |
Shielded twisted (Belden 8441 or equivalent) |
|
Permissible conductor cross-section |
0.4–1.5 mm2 |
|
Interconnection limit on inputs Z3, Z4, and Z5 (to downstream devices) |
15 devices |
|
Interconnection limit on outputs Z1 and Z2 (to upstream devices) |
5 devices |
The following figure shows the connection of the RC filter (part number LV434212).

Testing the ZSI Function
Test connection and operation of ZSI using EcoStruxure Power Commission software and the Service Interface.