LED Indication
Local Indicator
The LEDs and their meaning depend on the type of MicroLogic trip unit.
|
Type of MicroLogic trip unit |
Description |
|---|---|
|
|
|
Operation of the Ready LED
The Ready LED (green) blinks slowly when the standard protection functions of the electronic trip unit are operational. It indicates that the trip unit is operating correctly.
For MicroLogic 5 and 6 trip units: the Ready LED blinks at a value equal to the sum of the circuit breaker current for each phase and the neutral above a limit value. This limit value is indicated above the Ready LED, on the front face of the MicroLogic trip unit.
The following table uses two examples to illustrate the comparison of the phase and neutral currents with the activation limit value of the Ready LED:
|
MicroLogic 5.2 trip unit, 40 A rating, 3-pole |
MicroLogic 5.3 trip unit, 400 A rating, 4-pole |
|---|---|
|
The limit value is 15 A. |
The limit value is 50 A. |
|
This limit value can be:
|
This limit value can be:
|
The MicroLogic 7 trip unit with integrated earth-leakage protection has an internal voltage power supply (in addition to the supply provided by the current transformers) to power the earth-leakage protection even when the current demand is low. The Ready LED blinks irrespective of the load, indicating that the standard protection functions are operational.
Operation of Pre-Alarm and Alarm LEDs (Electrical Distribution Protection)
The pre-alarm (orange LED) and alarm (red LED) indications trip as soon as the value of one of the phase currents exceeds 90% and 105% respectively of the Ir pickup setting:
-
Pre-alarm
Exceeding the pre-alarm threshold at 90% of Ir has no effect on the long-time protection.
-
Alarm
Crossing the alarm threshold at 105% of Ir activates the long-time protection with a trip time delay that depends on:
-
The value of the current in the load
-
The setting of the time delay tr
-
Operation of Alarm LEDs (Motor Protection)
The alarm indication (red LED) trips as soon as the value of the motor thermal image exceeds 95% of the Ir pickup setting.
Crossing the threshold of 95% of Ir is a temperature alarm: long-time protection is not activated.