DOCA0188EN-03

Maintenance Indicators

BSCM Modbus SL/ULP Counters

The counters embedded in the BSCM Modbus SL/ULP module generate information relating to the number of volt-free contact operations. These volt-free contacts qualify:

  • The number of open/close operations (OF contact) and open on a fault operations (SD and SDE contacts) on the ComPacT NSX circuit breaker

  • The number of close, open, and reset operations on the motor mechanism

MicroLogic Trip Unit Counters

Access the maintenance counters embedded in the MicroLogic trip unit with the communication network.

  • Counters are assigned to each type of protection:

    • Long-time protection

    • Short-time protection

    • Instantaneous protection

    • Ground-fault protection

    • Earth-leakage protection

    • Jam motor protection

    • Phase unbalance protection

    • Long-start motor protection

    • Underload motor protection

  • Ten counters are assigned to the alarms associated with measurements. These counters reset if the alarm is reconfigured.

  • One counter indicates the number of operating hours. This counter is updated every 24 hours.

  • Four counters are assigned to the load profile: Each counter counts the number of operating hours per loading section (for example, one counter indicates the number of operating hours for the loading section 50–79% of In).

  • Six counters are assigned to the temperature profile: each counter counts up the number of operating hours per temperature section (for example, one counter indicates the number of operating hours for the temperature section 60–74 °C (60–165 °F)).

  • Use maintenance counters to enter quantitative information about operations performed on the MicroLogic trip unit (such as the number of push-to-trip tests) or the status of the MicroLogic trip unit (such as the number of Err screens or protection setting lock/unlock operations).

  • One counter indicates the amount of wear on the circuit breaker contacts as a percentage. When this figure reaches 100%, the contacts must be changed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?