Short-Time Protection
Presentation
Short-time protection on MicroLogic 5, 6, and 7 trip units protects all types of electrical distribution applications against short-circuit currents.
It is identical for MicroLogic 5, 6, and 7 trip units.
Operating Principle
Short-time protection is definite time:
-
It incorporates the possibility of an I2t inverse time curve function.
-
It is set using the Isd pickup and the tsd trip time delay.
Setting the Short-Time Protection (MicroLogic 5)
Set the Isd pickup:
-
With the MicroLogic trip unit Isd dial to preset the value and the keypad to fine-tune the value
-
With EcoStruxure Power Commission software (password-protected)
-
By sending a setting command using the communication network (password-protected)
Set the tsd time delay:
-
With the keypad on the MicroLogic trip unit
-
With EcoStruxure Power Commission software (password-protected)
-
By sending a setting command using the communication network (password-protected)
The tsd time delay setting includes activation/deactivation of the I2t function.
Setting the Short-Time Protection (MicroLogic 6 and 7)
Set the Isd pickup and tsd time delay:
-
With the keypad on the MicroLogic trip unit
-
With EcoStruxure Power Commission software (password-protected)
-
By sending a setting command using the communication network (password-protected)
The tsd time delay setting includes activation/deactivation of the I2t function.
Isd Pickup Setting Values
The Isd pickup setting value is in multiples of Ir.
The default Isd pickup setting value is 1.5 x Ir (minimum dial value).
The following table shows the setting values (preset by a dial) and setting ranges (set on the keypad) of the Isd pickup:
|
Type of setting |
Value or setting range (x Ir) |
||||||||
|---|---|---|---|---|---|---|---|---|---|
|
Preset by a dial (MicroLogic 5) |
1.5 |
2 |
3 |
4 |
5 |
6 |
7 |
8 |
10 |
|
Setting range on the keypad (1) Increment: 0.5 x Ir |
1.5 |
1.5–2 |
1.5–3 |
1.5–4 |
1.5–5 |
1.5–6 |
1.5–7 |
1.5–8 |
1.5–10 |
|
(1) For MicroLogic 6 and 7 trip units, the setting range value on the keypad is 1.5–10 x Ir. |
|||||||||
The accuracy range is +/-10%.
tsd Time Delay Setting Values
The following table indicates the setting values for the tsd time delay in seconds (s) with the I2t function active (I2t ON) or not active (I2t OFF). The associated hold and breaking times are shown in milliseconds (ms):
|
Function |
Setting value |
||||
|---|---|---|---|---|---|
|
tsd with I2t OFF (s) |
0 |
0.1 |
0.2 |
0.3 |
0.4 |
|
tsd with I2t ON (s) |
– |
0.1 |
0.2 |
0.3 |
0.4 |
|
Hold time (ms) |
20 |
80 |
140 |
230 |
350 |
|
Maximum breaking time (ms) |
80 |
140 |
200 |
320 |
500 |
The default tsd time delay setting value is 0 s with I2t OFF.
I2t Inverse Time Curve Function
Use the I2t inverse time curve function to improve circuit breaker coordination. Use it when a protection device using inverse time only is installed downstream, for example a fuse protection device.