Setting of the MicroLogic Protection Functions
WARNING |
|---|
|
HAZARD OF NUISANCE TRIPPING OR FAILURE TO TRIP
Protection setting adjustments must be done by qualified
electrical personnel.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Setting a Protection Function Using a Dial
Use an adjustment dial to set the following protection functions:
-
The Ir and Isd pickups for MicroLogic 5 trip unit
-
The Ir and Ig pickups for MicroLogic 6 trip unit
-
The Ir and IΔn pickups for MicroLogic 7 trip unit with integrated earth-leakage protection
Turning a dial results simultaneously in:
-
Selection of the screen for the protection function assigned to the dial
-
Unlocking (if necessary) the padlock (the navigation interface is in protection function setting mode)
-
Setting the protection function assigned to the dial to the value indicated on the dial and on-screen.
Setting a Protection Function on the Keypad
Use the keypad to fine-tune the protection function:
-
The setting value cannot exceed that indicated by the dial.
-
All the protection function settings are accessible on the keypad.
Press the
key successively to scroll
through the protection function screens. Scrolling is cyclical.
Navigate through the protection function settings with the
and
navigation keys.
-
Use the
key to select the function
to set:-
The up arrow indicates the selected function.
-
The down arrow indicates phase. Multiple down arrows indicate all phases set to the same value (except for the neutral protection setting).
-
Scrolling is cyclical.
-
-
Set the protection functions on the keypad with the
keys. The associated navigation arrows indicate the setting options:
Confirmation of Setting
The value of a protection function set on the keypad must be:
-
validated by pressing the
key once (the pictogram blinks on the display) -
then confirmed by pressing the
key again (the text is displayed for 2 s).
Example of Presetting a Protection Function Using a Dial
The following table illustrates presetting and setting the long-time protection Ir pickup on a MicroLogic 5.2 trip unit rated 100 A.
Press the
key to scroll through the
metering screens.
Press the
,
and
navigation keys to select the metering screen
for each of the phases.
|
Step |
Action |
Using |
Display |
|---|---|---|---|
|
1 |
Set the Ir dial to the maximum value (the padlock unlocks automatically). The down arrows indicate all three phases (the setting is identical on each phase). |
||
|
2 |
Turn the Ir dial to the setting above the value required. |
||
|
3 |
Presetting is complete:
|
||
|
4 |
Set the exact value required for Ir on the keypad (in increments of 1 A). |
||
|
5 |
Validate the setting (the pictogram blinks). |
||
|
6 |
Confirm the setting. The confirmation is displayed for 2 s. |
||
Example of Setting a Protection Function on the Keypad
The following table illustrates setting the long-time protection tr time delay on a MicroLogic 5.2 trip unit.
Press the
key to scroll through the
screens.
Press the
,
and
navigation keys to select the screen for each
of the phases.
Verification of the Protection Function Setting
In Protection function setting mode, a setting can be a relative value.
In Protection function readout mode, the setting is an actual value (for example in amps).
For example, to determine the actual value of a function currently being set as a relative value before validating the setting:
Example of Verification of a Protection Function Setting
The following table illustrates as an example the verification of the setting for the short-time protection Isd pickup on a MicroLogic 5.2 trip unit currently being set:
|
Step |
Action |
Using |
Display |
|---|---|---|---|
|
1 |
The display is in Setting mode on the Isd function: |
– |
|
|
2 |
Lock the setting: |
||
|
3 |
Unlock the setting: |
WARNING