DOCA0188EN-03

Description of the BSCM Modbus SL/ULP Module

Presentation

The BSCM Modbus SL/ULP module with commercial reference LV434220 is a Breaker Status Control Module that can be used to communicate data via:

  • Modbus Serial Line communication network

  • ULP communication network

The following data is exchanged:

  • OF and SDE circuit breaker states from the BSCM Modbus SL/ULP module

  • SD circuit breaker state from SD auxiliary contact for BSCM Modbus SL/ULP module or NSX cord (if present)

  • Control instructions for the communicating motor mechanism (if present): opening, closing, and resetting

  • Information to assist the operator: storage of the last 10 events

When connected to a MicroLogic 5, 6 or 7 trip unit, the BSCM Modbus SL/ULP module gives access to MicroLogic data.

The BSCM Modbus SL/ULP module can be used in the following modes:

  • Modbus SL only mode

  • Modbus SL and ULP mode

  • ULP only mode

If the BSCM Modbus SL/ULP module is used in Modbus SL only mode or in Modbus SL and ULP mode, the MicroLogic 5 or 6 trip units can be used to:

IMPORTANT:
  • The BSCM Modbus SL/ULP module Modbus parameters can be configured on MicroLogic 5 and 6 trip units with firmware version greater than or equal to 001.008.003.

  • The BSCM Modbus SL/ULP module Modbus parameters are not available on MicroLogic 7 trip units

For more information about the BSCM Modbus SL/ULP module, refer to DOCA0187•• ComPacT NSX - Circuit Breakers and Switch-Disconnectors 100–630 A - User Guide.

Description

  1. Port for BSCM Modbus SL cord

  2. Modbus address selector rotary switch

  3. Port for communicating motor mechanism

  4. ULP status LED

  5. Modbus status LED

  6. Port for MicroLogic 5, 6, or 7 trip unit

  7. Port for NSX cord or SD auxiliary contact for BSCM Modbus SL/ULP module

  8. OF contact

  9. SDE contact

  10. Cable to connect the BSCM Modbus SL/ULP module to the NSX cord or SD auxiliary contact for BSCM Modbus SL/ULP module

  11. Cable to connect the BSCM Modbus SL/ULP module to a MicroLogic 5, 6, or 7 trip unit

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?