Neutral Protection
Presentation
Neutral protection on MicroLogic 5, 6, and 7 trip units protects all types of electrical distribution applications against overload and short-circuit currents.
It is available on:
-
MicroLogic 5, 6, and 7 trip units for 4-pole circuit breakers
-
MicroLogic 5 and 6 trip units with ENCT option for 3-pole circuit breakers
Description
Normally, the phase protection protects the neutral conductor (if it is distributed and identical to the phases in size, that is, full neutral).
The neutral must have specific protection if:
-
It is reduced in size compared to the phases
-
Nonlinear loads generating third order harmonics (or multiples thereof) are installed
It may be necessary to switch off the neutral for operational reasons (multiple source diagram) or safety reasons (working with power off).
To summarize, the neutral conductor can be:
-
Non-distributed (3-pole circuit breaker)
-
Distributed, not switched off and not protected (3-pole circuit breaker)
-
Distributed, not switched off but protected (3-pole circuit breaker with ENCT option)
-
Distributed, switched off and protected (4-pole circuit breaker)
ComPacT NSX circuit breaker trip units are suitable for all protection types.
|
Circuit breaker |
Possible types |
Neutral protection |
|---|---|---|
|
3-pole circuit breaker |
3P, 3D |
None |
|
3-pole circuit breaker with ENCT option |
3P, 3D |
None |
|
3P, 3D + N/2 |
Half neutral |
|
|
3P, 3D + N |
Full neutral |
|
|
3P, 3D + OSN |
Oversized neutral |
|
|
4-Pole Circuit Breaker |
4P, 3D |
None |
|
4P, 3D + N/2 |
Half neutral |
|
|
4P, 4D |
Full neutral |
|
|
4P, 4D + OSN |
Oversized neutral |
|
|
P: Pole; D: Trip unit; N: Neutral protection |
||
Operating Principle
Neutral protection has the same characteristics as phase protection:
-
Its pickup is in proportion with the long-time Ir and short-time Isd protection pickups.
-
It has the same trip time delay values as the long-time Ir and short-time Isd protections.
-
Its instantaneous protection is identical.
Setting the Neutral Protection
4-pole trip unit
Set the IN pickup:
-
With the keypad on the MicroLogic trip unit
-
With EcoStruxure Power Commission software (password-protected)
-
By sending a setting command using the communication network (password-protected)
3-pole trip unit
Set the neutral declaration and the IN pickup:
-
With the keypad on the MicroLogic trip unit
-
With EcoStruxure Power Commission software (password-protected)
-
By sending a setting command using the communication network (password-protected)
Neutral Protection Setting Value
MicroLogic 5, 6, and 7 trip units incorporate the OSN (Oversized Neutral) function, which manages protection of the neutral conductor when third-order harmonic currents (and multiples thereof) are present.
The following table shows the setting values of the neutral long-time protection and neutral short-time protection pickups, according to the value of the IN/Ir function:
|
IN/Ir function |
Long-time pickup value Ir(IN) |
Short-time pickup value Isd(IN) |
|
|---|---|---|---|
|
OFF |
N/A |
N/A |
|
|
0.5 (1) |
Ir/2 |
Isd/2 |
|
|
1 |
Ir |
Isd |
|
|
(1) For the MicroLogic 7 trip unit with 40 A rating, the IN/Ir = 0.5 setting is not available. |
|||
The setting values are identical for the phases, the neutral long-time, and short-time protection time delays.
The following table details the setting values of the neutral protection pickups (set to OSN) according to the phase protection pickup Ir setting and the In rating of the 4-pole trip unit.
|
Ir/In values |
Long-time pickup value Ir(IN) |
Short-time pickup value Isd(IN) |
|
|---|---|---|---|
|
Ir/In < 0.63 |
1.6 x Ir |
1.6 x Isd |
|
|
0.63 < Ir/In < 1 |
In |
In x Isd/Ir |
|
Selection of the ENCT Option
The ENCT option is an external neutral CT for a 3-pole MicroLogic 5 or 6 trip unit.
The following table indicates the part number for the ENCT option installed according to the In rating of the MicroLogic trip unit or the need for OSN protection:
|
In rating (A) |
Neutral protection limited to In |
OSN neutral protection > In |
|---|---|---|
|
40 |
LV429521 |
LV429521 |
|
100 |
LV429521 |
LV429521 |
|
160 |
LV430563 |
LV430563 |
|
250 |
LV430563 |
LV432575 |
|
400 |
LV432575 |
LV432575 |
|
630 |
LV432575 |
No (1) |
|
(1) For the 630 A rating, the OSN function is limited to In (= 630 A). |
||
Installing the ENCT Option
|
Step |
Action |
|---|---|
|
1 |
Connect the neutral conductor to the ENCT option primary (terminals H1, H2). |
|
2 |
Remove (if existing) the jumper, between terminals T1 and T2 of the MicroLogic trip unit. |
|
3 |
Connect the ENCT option secondary (terminals T1, T2) to terminals T1 and T2 of the MicroLogic trip unit. |
|
4 |
Declare the ENCT option when setting the protection functions for the MicroLogic trip unit. |