Navigation Principles
Lock/Unlock the Settings
The settings are locked when the transparent cover is closed and sealed to prevent access to the adjustment dials and the locking/unlocking microswitch.
A pictogram on the display indicates whether the settings are locked:
To unlock the settings:
-
Open the transparent cover
-
Press the lock/unlock microswitch or turn one of the adjustment dials
To lock the settings, press the lock/unlock microswitch again.
The settings also lock automatically five minutes after pressing a key on the keypad or turning one of the dials on the MicroLogic trip unit.
Trip Unit Modes
Information displayed on the MicroLogic display is based on its mode.
The modes available depend on:
-
Whether the settings are locked
-
The trip unit version (3-pole or 4-pole)
-
The trip unit type (MicroLogic 5, 6 or 7)
The combination of pictograms defines the mode.
The following tables show the possible modes:
|
Pictograms |
|
|---|---|
|
|
|
Peak demand readout and reset |
|
|
Protection function readout |
|
|
Neutral status readout (3-pole MicroLogic trip unit) |
|
|
BSCM Modbus SL/ULP module setting readout (MicroLogic 5/6 trip units only) |
Mode Selection
Select the required mode by successive
presses on the
key:
-
The modes scroll cyclically.
-
Press the lock/unlock microswitch to switch between readout mode and setting mode.
Screensaver
The screensaver displays the instantaneous current passing through the most heavily loaded phase (Instantaneous measurement readout mode).
The MicroLogic display automatically reverts to a screensaver:
-
In padlock locked mode, 20 seconds after the last action on the keypad
-
In padlock unlocked mode, 5 minutes after the last action on the keypad or dials