Alarm Monitoring of the cos ϕ and Power Factor
Managing the cos ϕ and Power Factor PF
Monitoring of the cos ϕ and power factor PF indicators depends on the sign convention selected for the power factor PF: IEEE or IEC convention.
Select the sign convention for the PF indicator:
-
With EcoStruxure Power Commission software (password-protected)
-
By sending a setting command using the communication network (password-protected)
The IEEE convention is the factory setting.
Indicator Maximum and Minimum Values
-
The maximum value of the PF MAX or (cos ϕ MAX) indicator is obtained for the smallest positive value of the PF (or cos ϕ) indicator.
-
The minimum value of the PF MIN or (cos ϕ MIN) indicator is obtained for the largest negative value of the PF (or cos ϕ) indicator.
Electrical Distribution Monitored According to IEEE Convention
The following example describes monitoring of the energy quality by the cos ϕ indicator.
The following table gives the history of the cos ϕ values of the load of a workshop downstream of a ComPacT NSX circuit breaker according to IEEE convention:
|
Time |
Evolution of the load |
IEEE convention |
||
|---|---|---|---|---|
|
cos ϕ |
cos ϕ MIN |
cos ϕ MAX |
||
|
t1 = 8 h 00 min |
Power startup |
- 0.4 |
- 0.4 |
- 0.4 |
|
t2 = 8 h 01 min |
Compensation system startup |
- 0.9 |
- 0.4 |
- 0.9 |
|
t3 = 9 h 20 min |
Power stops |
+ 0.3 |
- 0.4 |
+ 0.3 |
|
t4 = 9 h 21 min |
Compensation system stops |
- 0.95 |
- 0.4 |
+ 0.3 |
Interpreting the cos ϕ MIN/MAX and the cos ϕ Values According to IEEE Convention
The cos ϕ MIN and cos ϕ MAX values correspond to the cos ϕ variation range for the load. This provides the user with information on how the equipment is performing from a cost point of view and allows the installation of compensation devices, if necessary. The cos ϕ MIN and cos ϕ MAX values can be accessed on the FDM121 display.
The load cos ϕ values indicate in real time any correction actions:
-
The absolute value of too low a negative cos ϕ (= - 0.4) indicates that capacitors need to be installed to increase the value of the equipment cos ϕ.
-
The value of too low a positive cos ϕ (= + 0.3) indicates that capacitors need to be removed to increase the value of the equipment cos ϕ.
The two alarms on the cos ϕ according to IEEE convention integrated in the MicroLogic trip unit are used to monitor the two critical situations automatically.
Electrical Distribution Monitored According to IEC Convention
The following table gives the history of the cos ϕ values of the load of a workshop downstream of a ComPacT NSX circuit breaker according to IEC convention:
|
Time |
Evolution of the load |
IEC convention |
||
|---|---|---|---|---|
|
cos ϕ |
cos ϕ MIN |
cos ϕ MAX |
||
|
t1 = 8 h 00 min |
Power startup |
+ 0.4 |
+ 0.4 |
+ 0.4 |
|
t2 = 8 h 01 min |
Compensation system startup |
+ 0.9 |
+ 0.9 |
+ 0.4 |
|
t3 = 9 h 20 min |
Power stops |
+ 0.3 |
+ 0.9 |
+ 0.3 |
|
t4 = 9 h 21 min |
Compensation system stops |
+ 0.95 |
+ 0.95 |
+ 0.3 |
Interpreting the cos ϕ MAX and the cos ϕ Values According to IEC Convention
The cos ϕ MAX value corresponds to the minimum value of the load cos ϕ, whether leading or lagging. This provides user information on how the equipment is performing from a cost point of view.
Do not use just the value of cos ϕ to decide whether to install inductances or capacitors to increase its value.
If a critical situation occurs, the alarm on the cos ϕ sends an alert according to IEC convention integrated in the MicroLogic trip unit. Use this alarm, associated with an alarm defining the type of load or the operating quadrant, to monitor the two critical situations automatically.
Setting the cos ϕ Alarms According to IEEE Convention
Monitor the cos ϕ indicator to manage the power:
-
When the power starts, too high a value of cos ϕ (lagging), for example higher than -0.6, results in penalties. The capacitive compensation value determines the value of the Qfund reactive power.
-
When the power stops, too low a value of cos ϕ (leading), for example less than +0.6, results in penalties. Disconnect the capacitive compensation element.
Two alarms monitor the indicators:
-
Alarm 124 (monitoring of the lagging cos ϕ) on an overvalue condition for operation in quadrant 1 (inductive reactive energy consumed)
-
Alarm 121 (monitoring of the leading cos ϕ) on an undervalue condition for operation in quadrant 4 (capacitive reactive energy consumed)
Set the parameters for monitoring the cos ϕ (alarms 121 and 124) according to IEEE convention with EcoStruxure Power Commission software.
Setting the SDx Outputs
The two alarms defined can each be associated with an SDx module output:
-
With output Out1, alarm code 124 (monitoring of the lagging cos ϕ)
-
With output Out2, alarm code 121 (monitoring of the leading cos ϕ)
Acknowledging the Out1 Screen
The Out1 screen can only be acknowledged if the alarm is no longer active.
After startup of the capacitive compensation, the alarm
is no longer active. Press the
key twice (validation and
confirmation) to acknowledge Out1 output.