DOCA0184EN-07

Complete the PrismaSeT Switchboard

To go to the mechanical elements section click the Distributions & FUsbutton > MECHANICAL ELEMENTS.

In the mechanical elements section, it’s possible to complete the switchboard with:

  • DIN rail and modular front plate for the reserve space

  • Earth bar

  • DIN rail and plains plats for terminal blocks

  • Front plate

A similar choice is proposed via a right-click, once the enclosure has been selected on the front face.

These four mechanical elements can be modified by selection on the front face and then a right click modify the installation system:

A modification regarding the height positioning is proposed for:

  • The DIN rail and modular front plate

  • The DIN rail and plains plats for terminal blocks

For the front plate, a modification of the height and the plate type (transparent, cut out) is proposed.

The button add front plates add automatically plates on the available space.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?