990-5936F-001

Connect the Load to the Branch Breakers

  1. Route the power cables from the load through the top or bottom right side of the PDU. Bottom cable entry is shown in illustration.
  2. For each power cable set:
    1. Connect the N cable to the N busbar.
    2. Connect the equipment grounding conductor/PE cable to the PE busbar.
    3. Route the power cables through the provided current transformers for the branch breaker. Check that the direction of the power cables matches the labels on the current transformers. The signal cables for the current transformers are preinstalled by the factory.
    4. Connect the power cables to the branch breaker.

    Front View of the PDU

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?