990-6318F-001

Configure the Network

  1. From the home screen on the display select Configuration > Network and select either TCP/IPv4, TCP/IPv6, Web Access, or FTP Server.
  2. Configure the following settings:
    1. TCP/IPv4: Enable IPv4 (if applicable), and select the Address Mode (Manual, DCHP, or BOOTP).
    2. TCP/IPv6: Enable IPv6 (if applicable), select Auto Configuration or Manual Configuration, and select the DHCPv6 Mode (Router controlled, Non-Address Information Only, Never, or Address and Other Information).
      NOTE: Tap Addresses to see all valid IPv6 addresses.
    3. Web Access: Enable Web (if applicable) and select the Access Mode (HTTP or HTTPS).
    4. FTP server: Enable FTP (if applicable).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.