990-6318F-001

Prepare for Top Cable Entry

DANGER
Hazard of electric shock, explosion, or arc flash
Do not drill or punch holes for cables or conduits with the gland plate installed and do not drill or punch holes in close proximity to the cabinet.
Failure to follow these instructions will result in death or serious injury.
  1. Remove the top gland plate.
  2. Remove the knockouts from the top gland plate for input cables and load cables as needed. Install conduits (not provided), if applicable. A blank gland plate is also provided if you need to make a different hole pattern.
  3. Reinstall the top gland plate.
  4. Install the provided Ethernet port (A) and Modbus port (B) in the top of the RPP. The internal Ethernet and Modbus signal cables are already prerouted to the top of the RPP.
    NOTE: In some RPP models, the Ethernet port (A) and Modbus port (B) are already preinstalled in the top of the cabinet.

    Top View

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.