990-6318F-001

Restore Default Configuration

  1. From the home screen on the display select Configuration > Restore Defaults.
  2. Select one of the below options:
    • Restart Network Interface: Select this option to restart network interface.
    • Reset All: Select this option to reset all settings to default. You can select to leave out the TCP/IP settings from the reset procedure.
    • Reset Only: Select this option if you only wish to reset parts of the settings to default values. You can select to reset the following settings: TCP/IP, Event Configuration, and Display Settings.
  3. When you have made your selection, tap OK to reset the selected settings to default.
  4. After the reset, it may be necessary to re-enable configuration via the display. Follow the below steps:
    1. Access the web interface for the network management, see Access a Configured Network Management Interface.
    2. At first user login, the user name and password are apc – you will be prompted to change the password at first login.
    3. Enable/disable communication protocols as needed.
    4. Create new users and configure user permissions.
    5. Enable the display access for user: Go to Config. > Security > Local Users and select Enable for Touch Screen and configure the PIN for the user.
    6. Configuration via the display is now enabled.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.