990-6318F-001

Connect the Load to the Branch Circuit Breakers

  1. Route the load power cables through the top or the bottom of the cabinet.
  2. For each load power cable set:
    1. Connect the ground cable to the ground terminal.
    2. Connect the N cable to the N terminal.
    3. Route the power cables through the current transformers for the branch circuit breaker.
      NOTICE
      Risk of equipment damage
      Route the power cables carefully through or near the current transformer strip to avoid damaging the current transformers. Do not assemble forcefully as this will create mechanical stress or deformation to the current transformers.
      Failure to follow these instructions can result in equipment damage.
    4. Connect the power cables to the branch circuit breaker.
    1. Panelboard 1.

    2. Panelboard 2 (if present).

  3. Fasten the load cables to the cable bridges in the left side and right side with cable ties.
    NOTE: Reinstall any protective plates and covers that were removed during the installation.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.