990-6318F-001

Remove a Branch Circuit Breaker

  1. Shut down the RPP, follow Shut Down the RPP.
  2. Open the front door.
  3. Disconnect the load cables from the branch circuit breaker.
    NOTICE
    Risk of equipment damage
    Route the power cables carefully through or near the current transformer strip to avoid damaging the current transformers. Do not assemble forcefully as this will create mechanical stress or deformation to the current transformers.
    Failure to follow these instructions can result in equipment damage.
  4. Remove the branch circuit breaker from the panelboard.
  5. Start up the RPP, follow Start Up the RPP.
  6. Delete the branch circuit breaker from the configuration via the display, follow Modify or Delete a Branch Circuit Breaker.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.