990-6318F-001

Alarm Messages

Display alarm text Description Corrective action
<LX> Phase Loss Alarm

Input supply phase L1, L2, or L3 loss is detected.

Check the input source and the affected phase.
A Circuit Breaker within the Unit has Tripped

A circuit breaker within the unit has tripped.

Check the circuit breaker and identify the cause of the tripping. Clear the tripping event and close the circuit breaker.
<Panel X> Branch <Breaker X> <Pole X> Apparent Power Below Minimum Branch circuit breaker X in Panel X is showing apparent power is below the minimum threshold at pole X. Check the power for the affected branch circuit breaker, evaluate the threshold setting, and adjust for your situation.
<Panel X> Branch <Breaker X> <Pole X> Apparent Power Overload

Branch circuit breaker X in Panel X is showing apparent power is above the maximum threshold at pole X.

Check the power for the affected branch circuit breaker, evaluate the threshold setting, and adjust for your situation.
<Panel X> Branch <Breaker X> <Pole X> High Current Alarm at Phase <LX>

Branch circuit breaker X in Panel X is showing phase L1, L2, or L3 current is above the high threshold at pole X.

Check the current for the affected branch circuit breaker, evaluate the threshold setting, and adjust for your situation.
<Panel X> Branch <Breaker X> <Pole X> Low Current Alarm at Phase <LX>

Branch circuit breaker X in Panel X is showing phase L1, L2, or L3 current is below the low threshold at pole X.

Check the current for the affected branch circuit breaker, evaluate the threshold setting, and adjust for your situation.
<Panel X> Branch <Breaker X> <Pole X> Maximum Current Alarm at Phase <LX>

Branch circuit breaker X in Panel X is showing phase L1, L2, or L3 current is above the maximum threshold at pole X.

Check the current for the affected branch circuit breaker, evaluate the threshold setting, and adjust for your situation.
<Panel X> Branch <Breaker X> <Pole X> Minimum Current Alarm at Phase <LX>

Branch circuit breaker X in Panel X is showing phase L1, L2, or L3 current is below the minimum threshold at pole X.

Check the current for the affected branch circuit breaker, evaluate the threshold setting, and adjust for your situation.
Input Breaker Open

The main input circuit breaker is open.                                                                        

Check the main input circuit breaker and adjust position or alarm settings depending on your situation.
Input Current High Alarm at Phase <LX>

The input phase L1, L2, or L3 current is above the high threshold.

Check the input current for the affected phase, evaluate the threshold setting, and adjust for your situation.
Input Current Low Alarm at Phase <LX>

The input phase L1, L2, or L3 current is below the low threshold.

Check the input current for the affected phase, evaluate the threshold setting, and adjust for your situation.
Input Current Maximum Alarm at Phase <LX>

The input phase L1, L2, or L3 current is above the maximum threshold.

Check the input current for the affected phase, evaluate the threshold setting, and adjust for your situation.
Input Current Minimum Alarm at Phase <LX>

The input phase L1, L2, or L3 current is below the minimum threshold.

Check the input current for the affected phase, evaluate the threshold setting, and adjust for your situation.
Input Voltage Maximum Alarm at Phase <LX>

The input phase L1, L2, or L3 voltage is above the maximum threshold.

Check the input voltage for the affected phase, evaluate the threshold setting, and adjust for your situation.
Input Voltage High Alarm at Phase <LX>

The input phase L1, L2, or L3 voltage is above the high threshold.

Check the input voltage for the affected phase, evaluate the threshold setting, and adjust for your situation.
Input Voltage Low Alarm at Phase <LX>

The input phase L1, L2, or L3 voltage is below the low threshold.

Check the input voltage for the affected phase, evaluate the threshold setting, and adjust for your situation.
Input Voltage Minimum Alarm at Phase <LX>

The input phase L1, L2, or L3 voltage is below the minimum threshold.  

Check the input voltage for the affected phase, evaluate the threshold setting, and adjust for your situation.
NMC Communication Lost with <X> Meter

Lost the local network management interface-to-input meter, output meter, or branch meter communication.

Check the signal cables. Check that the meter is energized and that it has been configured correctly — use the power meter documentation supplied with the power meter. If the alarm persists, contact Schneider Electric.
Input Active Power Phase <LX> Overload

The input active power for phase L1, L2, or L3 is above the selected high threshold.

Check the input power for the affected phase, evaluate the threshold setting, and adjust for your situation.
Input Apparent Power Phase <LX> Below Normal

The input apparent power for phase L1, L2, or L3 is below the selected minimum threshold.

Check the input power for the affected phase, evaluate the threshold setting, and adjust for your situation.
Input Apparent Power Phase <LX> Overload

The input apparent power for phase L1, L2, or L3 is above the selected maximum threshold.

Check the input power for the affected phase, evaluate the threshold setting, and adjust for your situation.
Input Frequency Out of Range

The input frequency is out of range.

Check the input frequency, evaluate the threshold setting, and adjust for your situation.
Input Power Factor Deviation Alarm at Phase <LX>

Input power factor deviation for phase L1, L2, or L3 exists.

Check the input power factor deviation for the affected phase, evaluate the threshold setting, and adjust for your situation.
Transient Voltage Surge Suppressor Alarm

Transient voltage surge suppressor system requires service.

Contact Schneider Electric to schedule a maintenance visit.
NOTE: Contact Schneider Electric if the RPP is operating correctly and the alarm persists, or if no root cause is found.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.