990-6318F-001

Modify or Delete a Branch Circuit Breaker

  1. From the home screen on the display select Configuration > Panel > Modify Breaker.
  2. Select the branch circuit breaker that must be deleted or modified using the parameters:
    1. Panel: Select which panelboard the branch circuit breaker is installed in (Panel 1 or Panel 2, if available).
    2. Layout: Select whether the branch circuit breaker is installed in the Odd or in the Even position on the panelboard. Odd is the left side of the panelboard and Even is the right side of the panelboard.
    3. Channel: Set which channel(s) the branch circuit breaker is installed in. Example channels 1,3,5 for a 3-pole branch circuit breaker. Already occupied channels are highlighted in blue in the channel list.
  3. Perform one of the following:
    • Tap on Delete Breaker to delete the branch circuit breaker.
    • Tap on Settings to modify the branch circuit breaker settings.
  4. On the first Settings page:
    1. Add the Load Identifier by typing in a name for the load connected to the branch circuit breaker.
    2. Enable or disable Alarm Generation for the branch circuit breaker by tapping Enable.
    3. Set the Apparent Power Thresholds for the branch circuit breaker for: Maximum and Minimum by tapping Enable and setting the percentage.
  5. Tap the > symbol to go to the next page.
  6. On the second Settings page:
    1. Set the Current Thresholds for the branch circuit breaker for: Maximum, High, Low, and Minimum by tapping Enable and setting the percentage.
  7. Tap OK to save your settings.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.