990-6318F-001

Configure a Branch Circuit Breaker

  1. From the home screen on the display select Configuration > Panel > Add Breaker.
  2. Configure the branch circuit breaker parameters:
    1. Panel: Select which panelboard the new branch circuit breaker is installed in (Panel 1 or Panel 2, if available).
    2. Layout: Select whether the new branch circuit breaker is installed in the Odd or in the Even position on the panelboard. Odd is the left side of the panelboard and Even is the right side of the panelboard.
    3. Tie: Set the number of poles on the branch circuit breaker (1-pole, 2-pole, or 3-pole).
    4. Channel: Set which L1 channel the new branch circuit breaker is installed in. L2 and L3 will be populated automatically. Example: Selecting channel 1 for a 3-pole branch circuit breaker will occupy channel 1,3,5. Already occupied channels are highlighted in red in the channel list.
    5. Rating: Set the circuit breaker rating current of the new branch circuit breaker.
  3. Tap on Add Breaker.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.