990-6318F-001

Connect the Input Cables

NOTE: The maximum allowed neutral cable size is 350 kcmil with the preinstalled cable lugs. For >350 to <500 kcmil neutral cable, replace the preinstalled neutral cable lug with kit TME69214, see Install the Neutral Mechanical Cable Lug Kit TME69214 (Option) for details.
  1. Route the input cables through the top or the bottom of the cabinet.
  2. Connect input cables from input source 1 (GEC, L1, L2, L3, N).
  3. Connect input cables from input source 2 (if present) (GEC, L1, L2, L3, N).
  4. Fasten the input cables to the cable bridges in the left side and right side with cable ties.
    NOTE: Reinstall any protective plates and covers that were removed during the installation.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.