990-6318F-001

Installation Procedure

WARNING
Tip hazard
The cabinet is top-heavy and can tip over. Move and store with care until it is time to anchor the cabinet to the floor and wall.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
  1. Anchor the Cabinet to the Floor and Wall.
  2. Perform one of the following:
  3. Only for >350 to <500 kcmil neutral cables with mechanical lugs: Install the Neutral Mechanical Cable Lug Kit TME69214 (Option)
  4. Connect the Input Cables.
  5. Connect the Load to the Branch Circuit Breakers.
  6. Connect the Modbus/Ethernet Cables.
  7. Final Installation.

For moving or decommissioning the RPP after installation has been completed, see Decommission or Move the RPP to a New Location.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.