990-6318F-001

Prepare for Bottom Cable Entry

DANGER
Hazard of electric shock, explosion, or arc flash
Do not drill or punch holes for cables or conduits with the gland plate installed and do not drill or punch holes in close proximity to the cabinet.
Failure to follow these instructions will result in death or serious injury.
NOTE: Bottom signal cable entry and/or bottom power cable entry is only possible if the RPP is installed on a raised floor or similar.
  1. Open the front door.
  2. Remove the bottom gland plate.
  3. Remove the knockouts from the bottom gland plate for input cables and load cables as needed. Install conduits (not provided), if applicable. A blank gland plate is also provided if you need to make a different hole pattern.
  4. Reinstall the bottom gland plate in rotated position to free the Ethernet and Modbus port openings.
  5. Install the provided Ethernet port (A) and Modbus port (B) in the bottom of the RPP. Reroute the internal Ethernet and Modbus signal cables from the top to the bottom of the RPP.
    NOTE: In some RPP models, the Ethernet port (A) and Modbus port (B) are already preinstalled in the top of the cabinet. Remove the ports and reinstall them in the bottom position as shown.

    Bottom View

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.