990-6318F-001

View the Status Information

  1. Select:
    • Status > Input > Input 1 to see the status for input 1.
    • Status > Input > Input 2 to see the status for input 2.

    Input Status

    Current The present input current from the AC utility power source per phase in amperes (A).
    Energy Usage The accumulated input energy (kWh) .
    Frequency The present input frequency in hertz (Hz).
    Breaker Status The present circuit breaker status, either Open or Closed.
    Voltage (phase-to-phase) The present phase-to-phase input voltage.
    Voltage (phase-to-neutral) The present phase-to-neutral input voltage.
    Apparent Power (total and per phase) The present apparent power input for each phase and total in kVA. Apparent power is the product of RMS (root mean square) volts and RMS amperes.
    Active Power The present active power (or real power) input for each phase and total in kilowatts (kW). Active power is the is the portion of the power flow that, averaged over a complete cycle of the AC waveform, results in net transfer of energy in one direction.
    Voltage THD (phase-to-neutral and phase-to-phase) The present harmonic distortion.
    Current Phase Angle Current phase angle displacement between the three phases.
    Power Factor (total and per phase) The present input power factor. Power factor is the ratio of Active power over Apparent Power.
    Frequency The present input frequency (Hz).
    Load % Percentage of load based on input circuit breaker rating.
    Neutral Current The present current in the neutral conductor.
    Average Current The average current of the three phases.
    Average Voltage (phase-to-phase and phase-to-neutral) The average voltage of the three phases.
  2. Select:
    • Status > Panel > Panel 1 Odd to see the status for the odd (left) side of panelboard 1.
    • Status > Panel > Panel 1 Even to see the status for the even (right) side of panelboard 1.
    • Status > Panel > Panel 2 Odd to see the status for the odd (left) side of panelboard 2.
    • Status > Panel > Panel 2 Even to see the status for the even (right) side of panelboard 2.

    Panel Status

    Current The present input current from the AC utility power source per phase in amperes (A).
    Max. Instantaneous Current The logged maximum current measured per phase by the power meter.
    Active Power (total and per phase) The present active power (or real power) input for each phase and total in kilowatts (kW). Active power is the is the portion of the power flow that, averaged over a complete cycle of the AC waveform, results in net transfer of energy in one direction.
    Apparent Power (total and per phase) The present apparent power input for each phase and total in kVA. Apparent power is the product of RMS (root mean square) volts and RMS amperes.
    Power Factor (total and per phase) The present input power factor. Power factor is the ratio of Active power over Apparent Power.
    Current THD The present harmonic distortion.
    Load % Percentage of load based on input circuit breaker rating.
    Breaker Rating Rating of the selected circuit breaker.
    CT Size Current transformer rating for the selected circuit breaker.
    Average Current The average current of the three phases.
    Max. Instantaneous Current Average The logged maximum current for three phase average measured by the power meter.
    Energy Usage The accumulated input energy (kWh) .
    Current THD Average The average of the present harmonic distortion.
  3. Select Status > System to see the status for the RPP system.

    System Status

    Input 1 Voltage (phase-to-phase) The present input voltage phase-to-phase from input power source 1 per phase in volts (V).
    Input 1 Current The present input current from input power source 1 per phase in amperes (A).
    Input 1 Breaker The present circuit breaker status for main input circuit breaker 1.
    Input 1 Frequency The present input frequency from input source 1 in Hertz (Hz).
    Input 1 Power Factor The present input power factor from input source 1.
    System Time The system time and date.
    Input 2 Power Factor The present input power factor from input source 2.
    Input 2 Frequency The present input frequency from input source 2 in Hertz (Hz).
    Input 2 Voltage (phase-to-phase) The present input voltage phase-to-phase from input power source 2 per phase in volts (V).
    Input 2 Current The present input current from input power source 2 per phase in amperes (A).
    Input 2 Breaker The present circuit breaker status for main input circuit breaker 2.
  4. Select Status > Active Alarms to see the status for the active alarms. For more information on active alarms, go to View the Active Alarms.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.