990-6318F-001

Install the Neutral Mechanical Cable Lug Kit TME69214 (Option)

NOTICE
Risk of equipment damage
Route the power cables carefully through or near the current transformer strip to avoid damaging the current transformers. Do not assemble forcefully as this will create mechanical stress or deformation to the current transformers.
Failure to follow these instructions can result in equipment damage.
NOTE: The maximum allowed neutral cable size is 350 kcmil with the preinstalled neutral mechanical cable lugs. For >350 to >500 kcmil neutral cable, replace the preinstalled neutral mechanical cable lugs with the larger mechanical cable lugs in kit TME69214.
  1. Remove the preinstalled mechanical cable lugs from the neutral busbars.
  2. Assemble the mechanical cable lug parts from kit TME69214.
  3. Install the mechanical lug assembly on the top and/or bottom of the neutral busbars with the provided screws.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.