990-6318F-001

Decommission or Move the RPP to a New Location

DANGER
hAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Electrical equipment must be installed, operated, serviced, and maintained only by qualified personnel.
Failure to follow these instructions will result in death or serious injury.
  1. Shut down the loads that the RPP is supplying.
  2. Shut down the RPP completely, see Shut Down the RPP.
  3. Lockout/Tagout the upstream input disconnect device in the OFF (open) position.
  4. Lockout/Tagout the main input circuit breaker(s) in the OFF (open) position.
  5. Lockout/Tagout the branch circuit breakers in the OFF (open) position.
  6. Measure for and verify ABSENCE of voltage on each input terminal before continuing.
    DANGER
    hAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
    Measure for and verify ABSENCE of voltage on each input terminal before continuing.
    Failure to follow these instructions will result in death or serious injury.

    Front View of the RPP

  7. Disconnect and remove all input cables from the RPP. See Connect the Input Cables for details.
  8. Disconnect and remove all load cables from the RPP. See Connect the Load to the Branch Circuit Breakers for details.
  9. Disconnect and remove the Modbus/Ethernet cable from the top or bottom of the RPP. See Connect the Modbus/Ethernet Cables for details.
  10. Reinstall any removed plates and covers.
  11. Reinstall the eye bolts and M12 nuts that were delivered with the RPP. See the receiving and unpacking manual for details.
    WARNING
    Hazard of dropping the cabinet
    • The cabinet must only be lifted and/or moved using the provided eye bolts as lifting points.
    • In case of hole deformation (ovalization) of the eye bolt, replace the eye bolt.
    • Use appropriate lifting equipment and lifting accessories (e.g. a crane with slings/chains) with a lifting capacity of minimum 300 kg (661 lbs).
    • Only use trained personnel to lift or move the cabinet.
    • Use appropriate personal protective equipment (PPE) such as helmets, gloves and safety shoes.
    • Follow all local regulations and guidelines for lifting equipment operations to ensure safety and compliance.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.

    Front View

  12. Attach lifting equipment to the eye bolts. This will prevent the cabinet from tipping over when the cabinet is no longer mounted to the wall/floor.

    Front View

  13. Remove the mounting hardware from the RPP, see Anchor the Cabinet to the Floor and Wall for details.
  14. Close and lock the front door.
  15. Lift the RPP using the eye bolts and appropriate lifting equipment.
  16. You can now move the RPP for short distances using the lifting equipment as instructed earlier in this procedure.
  17. For transport over longer distances:
    WARNING
    Tip hazard
    The cabinet is top-heavy and will tip over when not mounted to the floor/wall or to a pallet.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
    WARNING
    Tipping hazard
    For transport over longer distances, ensure:
    • that personnel performing the transport have necessary skill and have received adequate training;
    • to use appropriate tools to safely lift and transport the RPP;
    • to protect the product against damage by using appropriate protection (like wrapping or packaging).
    Failure to follow these instructions can result in death, serious injury, or equipment damage.

    Transportation requirements:

    • Mount the RPP in a vertical position in the center of a suitable pallet with minimum dimensions: 1070 x 1070 mm (42 in x 42 in). The pallet must be suitable for the weight of the RPP. The RPP weighs 200-250 kg (441-551 lbs).

    • Use appropriate means of fixation to mount the RPP to the pallet.

    • The original shipping pallet in combination with the original transportation brackets can be reused, if in undamaged condition.

    DANGER
    TIPPING hazard
    • The RPP must be appropriately fixed to the pallet immediately after being placed on the pallet.
    • The fixation hardware must be strong enough to withstand vibrations and shocks during loading, transport, and unloading.
    Failure to follow these instructions will result in death or serious injury.
  18. Perform one of the following:
    • Decommission the RPP, OR
    • Move the RPP to a new location to install it.
  19. Only for installing the RPP in a new location: Follow the installation manual to install the RPP in the new location. See Installation Procedure for installation overview.
  20. DANGER
    hAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
    Start-up must only be performed by qualified personnel.
    Failure to follow these instructions will result in death or serious injury.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.