990-6318F-001

Anchor the Cabinet to the Floor and Wall

DANGER
Hazard of electric shock, explosion, or arc flash
Cover the cabinet while drilling the anchoring holes in the floor and wall to avoid dust in the cabinet.
Failure to follow these instructions will result in death or serious injury.
WARNING
Tip hazard
The cabinet must be anchored to the floor and wall/structural frame similar to a wall/to another cabinet (back to back) to avoid tipping.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

The cabinet must be anchored to the floor (A) and to the wall/structural frame similar to a wall (B), or to the floor (A) and to another cabinet (C) in a back-to-back installation.

Cabinet Installed against a Wall and Cabinet in Back-to-Back Installation

  1. Drill anchoring holes in the floor according to the overview.

    Floor Anchoring Hole Overview

  2. For installation up against a wall or structural frame similar to a wall: Drill anchoring holes in the wall according to the overview. Note different dimensions between RPP models.

    Wall Anchoring Hole Overview

  3. Lift the cabinet into position using appropriate lifting equipment connected to the eye bolts.
    WARNING
    Hazard of dropping the cabinet
    • The cabinet must only be lifted and/or moved using the provided eye bolts as lifting points.
    • In case of hole deformation (ovalization) of the eye bolt, replace the eye bolt.
    • Use appropriate lifting equipment and lifting accessories (e.g. a crane with slings/chains) with a lifting capacity of minimum 300 kg (661 lbs).
    • Only use trained personnel to lift or move the cabinet.
    • Use appropriate personal protective equipment (PPE) such as helmets, gloves and safety shoes.
    • Follow all local regulations and guidelines for lifting equipment operations to ensure safety and compliance.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.

    Front View

  4. Anchor the cabinet to the floor with the provided 1/2 inch bolts.
  5. Anchor the cabinet to the wall, structural frame similar to a wall, or to the cabinet behind it with the provided 3/8 inch bolts.
  6. Open the door and remove the eye bolts, the M12 nuts, and the acrylic protection sheet from the top of the cabinet. Save the eye bolts and M12 nuts for future use.

    Front View

  7. Install the top gland plate (removed during unpacking of the cabinet).
    NOTE: The top gland plate has to be removed to prepare for top power cable entry. If your system has top power cable entry, see Prepare for Top Cable Entry.

    Front View

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.