990-6318F-001

User Interface

  1. Power meters

  2. Main input device(s)

  3. Display*

  4. Branch circuit breakers

  5. Status LEDs

  6. Display reset button

  7. Network connection LED:

    • Solid green: The system has valid TCP/IP settings.

      See Configure the Network.

    • Flashing green: The system does not have valid TCP/IP settings.

    • Solid orange: The display is inoperable. Contact Schneider Electric.

    • Flashing orange: The system is making BOOTP requests.

      See Configure the Network.

    • Alternately flashing green and orange: If the LED is alternately flashing slowly, the system is making DHCP requests.

      See Configure the Network.

      If the LED is alternately flashing rapidly, the system is starting up.

    • Off: The display is not receiving input power or the display is inoperable.

  8. LED for indication of network connection type:

    • Solid green: The system is connected to a network operating at 10 Megabits per second (Mbps).

    • Flashing green: The system is receiving or transmitting data packets at 10 Megabits per second (Mbps).

    • Solid orange: The system is connected to a network operating at 100 Megabits per second (Mbps).

    • Flashing orange: The system is receiving or transmitting data packets at 100 Megabits per second (Mbps).

    • Off: One or more of the following exists: The display is not receiving input power, the cable that connects the system to the network is disconnected, the device that connects the system to the network is turned off, or the display is inoperable. Check the connections and if the LED remains off, contact Schneider Electric.

  9. Display configuration port

  10. USB port.

  11. Ports reserved for service*

Overview of Status LEDs

Power LED: The RPP is powered when the LED is illuminated. Firmware is being updated when the LED is flashing.
Check log LED: When the LED is illuminated, a new entry has been made in the event log.
Alarm LED: When the LED is illuminated, there is an alarm condition in the RPP system.

Display Symbols

Symbol

Description

The locked home button appears when the system is locked by a password protection. Tap this button to go to the home screen of the display.

The unlocked home button appears when the system has been unlocked using the password. Tap this button to go to the home screen of the display.

Tap the OK button to confirm your selections and exit the current screen.

Tap the ESC button to cancel your changes and exit the current screen.

Tap the filter button to set up the filters for your logs.

Tap the recycle bin button to clear the log.

Menu Tree

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.