Local Remote Display (LRDH)
Refer Local Remote Display Installation Sheet (MFR40472) for information on product contents, installation, configuration, setup, and specification.
Using Local Remote Display, the hospital staff can understand whether the electrical installation is operating normal or on fault. The fault is displayed as a message on the device along with the instructions to follow when fault occurs.
The following messages are displayed on the device and its description:
-
Follow the instructions displayed whenever you see these message screens except Installation Ready.
-
On any message except Installation Ready, the buzzer turns ON. Touch the
icon to turn OFF the buzzer.
-
If multiple messages are displayed, touch and hold the
and
icons to navigate and view all the displayed messages.
-
Installation Ready
This message displays when there is no fault in the system.
-
Insulation Fault
This message displays when the system insulation is less than the set threshold.
You cannot acknowledge this message. This message continues to display until the system insulation is greater than the set threshold.
-
Transformer Overload
This message displays when the system load current is greater than the set threshold.
You cannot acknowledge this message. This message continues to display until the system load current is less than the set threshold.
-
Transformer Overheat
This message displays when the temperature sensor of the system transformer trips due to overheating.
You cannot acknowledge this message. This message continues to display until the system transformer temperature is less than the sensor threshold.
-
Product Error
This message displays when the connected devices encounter an unknown error.
You cannot acknowledge this message. Contact Schneider Electric customer care representative for support.
-
System Error
This message displays when there is an issue in the system.
You cannot acknowledge this message. This message continues to display until the system recovers from the issue.
-
Communication Error
This message displays when the connected devices encounter communication issues.
To acknowledge this message, touch and hold the
icon for 2 seconds and release it. Check the communication settings of the highlighted devices.
NOTE: If the existing communication error is not fixed in 1 minute, this message displays again.