Hospital Remote Panel (HRP)
The HRP installed in the operating theater enables the hospital staff to understand whether the installation is operating or whether there is a fault as per the following cases:
-
Insulation fault affecting the electrical equipment of the operating theater
-
Electrical fault following tripping of a protective circuit breaker or overloading of a current transformer
The physical description of the HRP is illustrated in the following figure:
| Number | Description |
|---|---|
| 1 | Yellow LED: Visual indication of an insulation fault |
| 2 | Green LED: Visual indication that the installation is operating |
| 3 | Red LED: Visual indication of an electrical fault (overload, overheating of the transformer, or tripping of a circuit breaker on fault) |
| 4 | Mute button |
| 5 | Push-button for testing the insulation monitoring system (daily test in accordance with standard IEC 60364-7-710) |
| 6 | Volume controller to adjust the alarm volume (Alarm volume is factory preset at 80 db. Use the volume controller to increase or decrease the volume).. |
| 7 | Connector |
The HRP is flush-mounted on a partition. See the following figure for mounting information:
The HRP is connected to the insulation alarm relay terminal block. See wiring diagram from the device to the HRP (Wiring diagram). The connector details of HRP is illustrated in the following figure:
The characteristics of the HRP is as follows:
| Characteristics | Value | |
|---|---|---|
| Mechanical Characteristics | ||
| Weight | 0.5 kg (1.1 lbs) | |
| Case | Plastic | Vertical mounting |
| Degree of protection | IP54 | |
| IK08 | ||
| Dimensions | Height | 170 mm (6.69 in) |
| Width | 170 mm (6.69 in) | |
| Depth | 20 mm (0.79 in) | |
| Audible alarm | Factory setting | 80 db (adjustable) |
| Durable markings | Tested with 99% Isopropyl Alcohol | |
| Electrical Characteristics | ||
| Auxiliary supply voltage | 24 V DC | 65 mA |
| Environment | ||
| Operating temperature | 0...40 °C | |
| Storage temperature | -25...+70 °C | |
| Maximum relative humidity | 90% | |
| Altitude | 3000 m (9842 ft) | |
| Standards | ||
| Compliant with | IEC 60364-7-710 | Medical facilities |
| IEC 61557-8 | Electrical safety | |
| IEC 60601-1 | Electrical medical equipment | |
| IEC 61010–1 | Electrical equipment safety | |