VIGED310023EN-06

Information icons

Icons in the information area of the LCD display provide information such as what menu is selected and the insulation alarm status.

The following table is profiled. Check for row profiling before updating any content
Icon Description
Main menu
  • System resistance (in the absence of an insulation fault)

  • Measurement parameters menu

Fault log menu (IM20-H)
Setting parameters menu and submenu
Display language selection menu
Product identification
Indication of an insulation or transformer fault alarm
Check for IFL12H row profiling

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?