VIGED310023EN-06

Mounting

  1. Position the upper slots on the rear of the device on the DIN rail.
  2. Press the device against the DIN rail until the locking mechanism engages.
    The device is fixed to the rail.
  3. Do the wiring and insert the terminal blocks as shown in the relevant wiring diagram (See Wiring diagram) and as appropriate for the type of device concerned (See Hardware overview).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?