VIGED310023EN-06

Example application: IM10-H and HRP

An example of IM10-H and HRP installed in the medical premises.

Because, HRP is installed in the operating room the monitoring system can collate and display all the information relating to the insulation alarms generated by the electrical installation.

The HRP connection with operation theater cabinet is illustrated in the following figure:

The HRP connection principle is illustrated in the following figure:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?