Monitoring of the transformer temperature
These bimetal type sensors open or close when the temperature exceeds their setpoint threshold. If the transformer is equipped with several sensors having several thresholds, the "alarm temperature" sensor must be used.
| NOTICE |
|---|
|
Equipment damage
Configure the device according to the type of sensor.
Failure to follow these instructions can result in equipment damage.
|
Since the temperature sensors are installed on each column of the transformer, their wiring depends on the sensor type:
-
Wire the NO bimetal temperature sensors (which close when the temperature exceeds the threshold) in parallel
-
Wire the NC bimetal temperature sensors (which open when the temperature exceeds the threshold) in series
Pt••• type temperature sensors are not compatible with the device.
When overheating trips the bimetal sensor, a transformer alarm is generated on the HMI of the device, on the HRP, Transformer Overheat message is displayed on the Local Remote Display, sent via the Modbus communication and the transformer alarm relay is activated.