Device overview
IMD applies low-frequency AC voltage between the power system and the ground to provide accurate insulation monitoring in complex applications. The insulation is then assessed on the basis of the current value returned. This method is used for all power system types - AC, DC, combined, rectified, with a variable speed drive, etc.
IM10-H, IM15H, and IM20-H offers the following features:
-
Insulation resistance display (R)
-
Detection of insulation faults in accordance with a configurable threshold
-
Detection of a lost connection (ground or injection)
IM15H and IM20-H offers these additional features:
-
Insulation fault log
-
Transformer monitoring:
-
Display of load current for secondary (as a percentage)
-
Threshold-based triggering of an alarm (as a percentage of nominal current)
-
Temperature alarm (bimetal contact)
-
IM20-H offers communication via the ModbusRS-485 protocol feature.