VIGED310023EN-06

Dismounting

  1. Disconnect the terminal blocks from the device.
  2. Use a flat screwdriver (≤ 6.5 mm (0.26 in)) and push down the locking mechanism to release the device.
  3. Lift the device up to free it from the DIN rail.
  4. Reinsert the terminal blocks and make sure that the correct positions on the device are observed (See Hardware overview).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?