EIO0000004348_00

Calibration

Calibrates the touch coordinates.

NOTE:
  • When connecting to one of our hosts, use this utility instead of the Windows® Calibration function.

  • Before running calibration, in the Windows display settings set the Scale and layout to 100% for the associated display. You cannot calibrate properly using other scaling settings.

When this product is connected to the Harmony P6 Panel Type, an icon for selecting the target display is displayed first. When you select an icon, the associated display flashes so you can identify which display to set up.

Front Display: Harmony P6 Panel Type
Extend Display: This product

Calibration screen instructions are different between analog resistive film and projected capacitive (P-CAP) displays. Perform calibration as per the screen instructions.

Analog resistive film display

Projected capacitive display

Commentaires
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.