0614CT1701

Product Selector

The ACB Product Selector provides a fast, secure and smart way of selecting and configuring LV circuit breaker ranges. It includes the selection of the basic frame, control unit, accessories and digital modules.

Compared to the traditional way for placing an order through Request for Quote (RFQ) forms, it brings the following benefits:

  • Intuitive and interactive interface eases and speeds up the device configuration.

  • Configuration rules are embedded, viable options are automatically filtered and completeness of the configuration is confirmed.

  • The confirmed feature file can be saved either locally or through web services, allowing future repeated or modified configuration to be done in a fraction of the time.

NOTE: All configurations are normally done using the ACB Product Selector. If you have difficulties accessing or using the product selector, contact Schneider Electric Customer Care Center or your Schneider Electric sales representatives for more information about ordering MasterPacT MTZ devices.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?