0614CT1701

MasterPacT MTZ QR Codes

MasterPacT MTZ circuit breakers have a QR code on the front cover of the circuit breaker control unit. Reading the QR code with a smartphone or tablet provides access to the device's characteristics, documents and downloads and the safe repository for authentication.

Safe Repository

The safe repository allows user access to circuit breaker configuration details such as the device's product code, serial number, and a high level Bill of Materials (BOM) format.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.