0614CT1701

Interlocks Catalog Numbers

Description

Door Interlock
Door Interlock MTZ1 Right and left-hand side of cradle (VPECD or VPECG) LV833172SP
Door Interlock MTZ2/3 Right and left-hand side of cradle (VPECD or VPECG) LV847914SP
Cable-type door interlock 1 complete assembly for MasterPacT MTZ2/MTZ3 fixed or drawout device LV848614SP
Mechanical Interlocking for Source Changeover for MTZ2/3.
Interlocking of 2 devices using connecting rods Choose 1 set of 2 adaptation fixtures (1 for each device)+1 set of rods Rod Interlock kit :1 set of 2 adaptation fixtures for MasterPacT MTZ2 or MTZ3 fixed or drawout device LV847930SP
1 set of 2 interlocking rods LV833210SP
Can be used with 1 MTZ2/3 fixed + 1 MTZ2/3 drawout. Note : the installation manual is enclosed. Interlocking of 2 devices using cables
  LV847926SP
Interlocking of 2 devices using cables Choose 2 adaptation sets (1 for each device +1 set of cables) 1 adaptation fixture for MasterPacT MTZ2/3 fixed devices LV847926SP
Cable mounting plate : 1 adaptation fixture for MasterPacT MTZ2/3 drawout devices LV847926SP
Cable interlock :1 set of 2 cables LV833209SP
Interlocking of 3 devices using cables Choose 3 adaptation (including 3 adaptation fixtures + cables) 3 sources, only 1 device closed, fixed or drawout devices LV848610SP
2 sources + 1 coupling, fixed or drawout devices LV848609SP
2 normal + 1 replacement source, fixed or drawout devices LV848608SP
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.