0614CT1701

MyPacT Online Software Tool

Go to MyPacT

MyPacT online software tool provides a fast, secure, and smart way of selecting and configuring LV circuit breakers. It includes the selection of the basic frame, control unit, accessories and digital modules. Compared with the traditional way of filling up order forms or specifying customer functions, it brings the following benefits:

  • state-of-the-art ergonomic, intuitive and interactive interface eases and speeds up the configuration

  • configuration rules are embedded, compatible options are automatically filtered and completeness of the configuration is checked. This results in compatible configurations and saves time fixing configuration errors.

  • configurations can be saved either locally or through cloud service. Repeated or modified configurations can be done in a fraction of the time.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.