0614CT1701

Neutral Sensors Catalog Numbers

External Sensor for Neutral Ground-Fault Protection (TCE)

External Sensor for Source Ground-Return Protection

MDGF

Neutral Sensor Parts

 

Catalog Number

Neutral Sensor Wiring Harness for MTZ1/2

LV848907SP

Neutral Sensor Wiring Harness for MTZ3

LV848906SP

MDGF/SGR (Source Ground Return) Sensor plug

External sensor (SGR)

Four MDGF sensors (phase + 1 neutral) are required for MTZ2; eight MDGF sensors are required for MTZ3. For SGR system only one sensor (neutral) is required for MTZ2; two sensors for MTZ3.

*

LV833579SP

MDGF summing module for MTZ2/3

LV848891SP

MasterPacT MTZ1 External Neutral Sensors

Used With Sensor Plug

External Neutral Sensor For General Use

Circuit breakers with standard neutral protection

400–1600 A

LV833576SP

Circuit breakers with oversized neutral protection *

400–1000 A

LV833576SP

1200–1250 A

LV834035SP

1600 A

LV834036SP

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.