0614CT1701

MicroLogic X Control Unit

Overview of MicroLogic X Control Unit

Overview of Available MicroLogic X Control Unit Protection Functions

The MasterPacT MTZ protection functions included in the control unit provide overcurrent, short-circuit, and ground-fault protection.

An embedded power meter offers the measurement parameters required to optimize energy management.

The optional digital modules offer upgrades to the Protection, Measurement, and Maintenance & Diagnostics functions.

The information processed and stored by the MicroLogic X control unit is accessible by:

  • The embedded human-machine interface (HMI) with colored backlight.

  • Using smartphones via Bluetooth™ technology and near-field communication (NFC).

  • Using an external personal computer (PC) through a universal serial bus (USB) connection.

Connection to Ethernet is achieved with dedicated interface modules: the Ethernet Interface (IFE) or the Embedded Ethernet Interface for Drawout MasterPacT MTZ device (EIFE).

Connection to the Modbus SL (RTU) is achieved with the Modbus Interface Module (IFM). For more information, consult Schneider Electric.

Layout of the MicroLogic X Control Unit

The MicroLogic X control unit’s basic protection functions are on a dedicated circuit and processor that is protected from disturbances.

In-depth diagnostics allows users to follow the status and operating condition of the circuit breaker in real time.

The backlit display will change colors for various states, providing a clear indication when attention is needed.

Information processed by the MicroLogic X control unit can be displayed on the embedded HMI, a smart device through Bluetooth technology or NFC, local front display (FDM128), communications such as Ethernet, and a PC through the USB connection.

MicroLogic X configuration is easily made through the EcoStruxure™ Power Commission Software.

MicroLogic X Control Unit Protection Functions

The MicroLogic X control unit is suitable for different systems of voltage, three or four wires up to 600 Vac, 50/60 Hz and for grounded systems.

Model

Protection

Catalog Number

Additional Features

   

MicroLogic 3.0 X

LI:
Long time
+ Instantaneous

LV848815FS

Digital Modules

MicroLogic 5.0 X

LSI:
Long-time
+ Short-time
+ Instantaneous

LV847609FS

Digital Modules

MicroLogic 6.0 X

LSIG:
Long-time
+ Short-time
+ Instantaneous
+ Ground-fault

LV847608FS

Digital Modules

Long-Time Overload Protection (ANSI 49RMS/51)

Long-time protection protects the conductors against overload currents. It is based on the true RMS current and is implemented independently for each phase and the neutral.

Thermal imaging is integrated into the long-time protection that models the heating and cooling cycles of the conductors.

Short-Time Short Circuit Protection (ANSI 50TD/51)

Short-time protection protects the installation against phase-to-phase, phase-to-neutral and phase-to-ground short circuits.

It is based on the true RMS current. It includes two characteristics depending on the status of the I2t setting:

  • When I2t is OFF, a definite time characteristic is selected.
    The protection trips with the time delay tsd as soon as the setting current Isd is exceeded.

  • When I2t is ON, an inverse time characteristic is selected.
    The protection operates with the inverse time characteristic up to 10 x Ir and with a definite time characteristic above 10 x Ir.

Short-time adjustment may be used to improve selective coordination for the electrical system. Zone-selective interlocking (ZSI) interconnects multiple trip units to provide total coordination for short-time protection.

Instantaneous Short Circuit Protection (ANSI 50)

Instantaneous protection protects the installation against phase-to-phase, phase- to-neutral and phase-to-ground short circuits.

The protection operates with a definite time characteristic.

It trips without additional time delay when the setting current Ii is exceeded. The protection offers two selectable tripping times:

  • Standard tripping time: 50 ms for applications requiring selectivity. Selectivity requires correctly sizing another circuit breaker installed downstream of the MasterPacT circuit breaker.

  • Fast tripping time: 30 ms (used when selectivity is not required).

Ground-Fault Protection (ANSI 50N-TD/51N)

Ground-fault protection can be achieved in two ways:

  • By performing the summation of the three phases and neutral currents.

  • By means of an external sensor (Source Ground Protection [SGR]*) installed around the cable connecting the transformer neutral point to ground. The SGR sensor is connected to the MicroLogic 6.0 X control unit through an MDGF interface module.

Replacement Parts and Accessories for MicroLogic X Control Units

Catalog Number

MicroLogic X Embedded Display (EHMI)

MicroLogic X embedded display & wireless card

LV850054SP

MicroLogic XI Embedded Display (EHMI)

MicroLogic X embedded display & wireless card

LV850054WWSP

MicroLogic X Battery + Transparent Cover


Battery (1 part)



LV833593SP


Transparent Cover (1 part) For MicroLogic X

LV850053SP

Transparent Cover with access to holes (1 part) for MicroLogic X

 

Transparent Cover with access to holes (1 part) for MicroLogic X

LV839453SP

Voltage Power Supply Module (VPS)

Voltage power supply module (VPS) for MicroLogic X

LV850060SP

Microswitches for MTZ1

Microswitches for MTZ circuit breakers

LV847906SP

USB Cable (miniUSB/USB) for MicroLogic X

   

LV850067SP

Mobile Power Pack for MicroLogic X (by APC)

   

LV850055SP

ZSI Interface module (restraint interface module)

120 Vac

 

LV848892SP

USB Cable for MicroLogic X Control Unit

USB Cable (miniUSB/USB) for MicroLogic X control unit / 1 part

Sensor Rating 400/1600 A

LV850067SP

Replacement Parts and Accessories for MicroLogic X Control Units

Catalog Number

External Sensors

External Sensor for Ground-Fault Protection (TCE)

Sensor rating 400/2000 A

Sensor rating 1000/4000 A

Sensor rating 4000/6300 A (MTZ3)

LV834035SP

LV834036SP

LV848182SP

Single sensor kit 2000/6300 A

LV848904SP

3 layer bus 2000 A

LV848905SP

Source Ground Return (SGR) Ground-Fault Protection

External Sensor (SGR)

LV833579SP

MDGF Summing Module

LV848891SP

Voltage Measurement Input (for Circuit Breakers Supplied via Bottom Terminals)


Voltage Measurement Input Fixed


LV847506

Drawout

LV848533

Protective Function Ratings

MicroLogic 3.0 X Control Unit

Long-Time

ANSI Code 49RMS/51

Current setting (A)

Ir = In x …

Ir = 0.4 In to In, 1 A increments

Tripping between 1.05 and 1.2 x Ir

Time setting

tr = 0.5 s to 24 s, step 0.5 s for 6 x Ir

Time setting example:
Time delay (s)

1.5 x Ir (+0/-30%)

12.5

25

50

100

200

300

400

500

600

6 x Ir (+0/-30%)

0.5*

1

2

4

8

12

16

20

24

7.2 x Ir (+0/-20%)

0.7*

0.69

1.38

2.7

5.5

8.3

11

13.8

16.6

Thermal memory

After tripping based on thermal imaging model

Instantaneous

ANSI Code 50

Pick-up (A) (±10%)

Ii= In x …

Ii = 1.5 In to 12 In, 0.5 In increments*

Operating time

Max resettable time:

20 ms

0 ms

Max breaking time:

50 ms

30 ms

MicroLogic 5.0 X / 6.0 X Control Unit

Long-Time

ANSI Code 49RMS/51

Current setting (A)

Ir = In x …

Ir = 0.4 In to In, step 1 A

Tripping between 1.05 and 1.20 Ir

Time setting

tr = 0.5 s to 24 s, 0.5 s increments for 6 Ir

Time setting example:
Time delay (s)

1.5 x Ir (+0/-30%)

12.5

25

50

100

200

300

400

500

600

6 x Ir (+0/-30%)

0.5*

1

2

4

8

12

16

20

24

7.2 x Ir (+0/-20%)

0.7*

0.69

1.38

2.7

5.5

8.3

11

13.8

16.6

Thermal memory

After tripping based on thermal imaging model

Short-Time

ANSI Code 50TD/51

Pick-up (A) (±10%)

Isd = Ir x …

Isd = 1.5 Ir to 10 Ir, 0.5 Ir increments*

Time setting tsd (s)

Settings

I2t Off

0

0.1

0.2

0.3

0.4

I2t On

-—

0.1

0.2

0.3

0.4

Operating time at 10xIr

I2t Off or I2t On

Max resettable time

20

80

140

230

350

Max break time

80

140

200

320

500

Instantaneous

ANSI Code 50

Pick-up (A) (±10%)

Ii = In x …

Ii = 2 to 15 In, 0.5 In increments, OFF protection*

Operating time

Max resettable time:

20 ms

0 ms

Max breaking time

50 ms

30 ms

MicroLogic 6.0 X Control Unit

Ground Fault

Ground Fault ANSI Code 50N-TD/51N

Pick-up (A) (±10%)

Ig = In x …

Ig = 0.2 In to 1200 A*, 0.1 In increments *

Time setting tg (s)

Settings

I2t Off

0

0.1

0.2

0.3

0.4

I2t On

-

0.1

0.2

0.3

0.4

Operating time (ms)

Non-tripping time

20

80

140

230

350

Max breaking time

80

140

200

320

500

Additional MicroLogic X Control Unit Functions

Neutral Overload Protection on Four-Pole Circuit Breakers

A four-pole circuit breaker neutral protection is set remotely:

  • Neutral protection set at unprotected.

  • Neutral protection set at 0.5 x Ir.

  • Neutral protection set at Ir.
    Neutral protection is greater than Ir, but lower than In and limited at 1.6 Ir phase.

For a three-pole circuit breaker used in a 4-wire circuit, the protection of the neutral requires an additional external neutral CT (ENCT). A long-time overcurrent characteristic is dedicated to the neutral protection.

Trip Coil Supervision (ANSI 74)

The MicroLogic X control unit continuously monitors the electrical continuity of the circuit breaker tripping coil. It generates an alarm if a problem is detected.

Lock-Out Function (ANSI 86)

If the circuit breaker is tripped from an overcurrent event or from one of the protective functions the circuit breaker is locked in the open position until it is reset manually or electrically. MasterPacT MTZ circuit breakers are also equipped with an interlocking function (see MasterPacT MTZ Locking and Interlocking Accessories).

Dual Settings

The MicroLogic X control unit is equipped with dual protection settings which allow the user to have a second set of protection settings. This allows users to easily switch between settings.

A typical application is to adjust the short-circuit protection when an installation can be supplied by two sources (grid / generator set) with different levels of available short-circuit current. The settings can be selected by one of the following means:

  • EcoStruxure Power Device App

  • by a digital input through the IO module

  • via Ethernet

  • from the embedded HMI

Overcurrent and Trip Cause Indications

Five LEDs are available on the front of the MicroLogic X control unit.

  1. The PreWarn/Warn LED is a bicolor LED with two functions:

    1. PreWarn/Warn LED changes to orange when I > 0.9 Ir

    2. Warn LED changes to red when I > 1.05 Ir

  2. The Ir LED is dedicated to long time overload protection, it changes to red when the protection trips.

  3. The Isd/Ii LED is dedicated to short-time and instantaneous short-circuit protection. It changes to red with a short-time or instantaneous overcurrent event.

  4. The Ig/IΔn LED is dedicated to ground-fault protection. It changes to red when that protection trips.

  5. The Op. LED is dedicated to the optional protections and changes to red when any of the optional protections trip.

The fault indication LEDs remains ON four hours after trip if not reset by the test/reset pushbutton. After four hours without reset it is possible to reactivate the trip indication LEDs by pushing the test/reset pushbutton.

The battery charge is continuously monitored.

Trip History

Trip history is captured and stored in the control unit, and can be retrieved and evaluated using Ecoreach™ software and the EcoStruxure Power Device App.

Each trip inside the trip history (except the last one) includes:

  • Type of protection that caused the trip: long-time (overload), short-time (short-circuit), instantaneous (short-circuit), ground fault.

  • Date and time of the fault.

The last 50 trip histories can also be retrieved by means of a PC running EcoStruxure Power Commission Software.

In addition, MicroLogic X control unit also logs:

  • Last electrical values measured before the fault (voltages, currents, frequency, current and voltage unbalance levels),

  • Tripping current during the fault just before the MasterPacT MTZ circuit breaker trip (phase, neutral and ground currents).

  • Protection settings.

The last trip may be retrieved through the NFC powerless wireless communication while the circuit breaker is open and the MicroLogic X control unit is not energized.

Protection Settings and Checking

The protection settings can be set by means of the embedded display, a smartphone via Bluetooth technology, or with EcoStruxure Power Commission Software running on a PC.

EcoStruxure Power Commission Software allows:

  • Setting and checking the protections.

  • Downloading current settings and uploading new settings.

  • Checking the circuit breaker operation.

  • Retrieving and displaying information processed by the MicroLogic X control unit:

    • Measurements

    • Alarms

    • Warnings

    • Diagnostics

  • Generating and storing reports.

Setting Change Traceability

Setting changes are recorded in the protection history, including:

  • Date and the time of the last setting change.

  • Previous settings and new settings.

The NFC wireless connection allows access to the active trip settings while the circuit breakers is Open and the MicroLogic control unit is not energized.

Setting Change Locking

The general configuration menu of the MicroLogic X control unit’s embedded display allows:

  • Enabling or disabling the protection setting change from the embedded display.

  • Enabling or disabling the protection setting change from external access:

    • Smartphone via Bluetooth technology

    • PC running EcoStruxure Power Commission Software

    • Ethernet and Modbus SL (RTU) communication.

Zone-Selective Interlocking (ZSI)

ZSI is a system designed to reduce the stress on electrical distribution equipment during short-circuit or ground-fault conditions. It uses previously-coordinated protection to reduce the fault tripping time while maintaining selectivity. Each version of the MicroLogic X control unit includes the ZSI function. The ZSI function is associated with short-time short-circuit protection and ground-fault protection.

The control unit detecting a fault sends a signal upstream and checks for a signal arriving from downstream. If there is a signal from downstream, the circuit breaker remains closed for the full duration of its tripping delay. If there is no signal from downstream, the circuit breaker opens immediately, regardless of the tripping-delay setting.

Zone selective interlocking can be implemented between all types of MasterPacT MTZ circuit breakers.

When ZSI connects MasterPacT MTZ circuit breakers with circuit breakers other than MasterPacT MTZ, it may be necessary to use a ZSI Interface Module.

Fault 1

Only circuit breaker A detects the fault. Because it receives no signal from downstream, it trips with no intentional delay, regardless of its tripping delay set to 0.3.

Fault 2

Circuit breakers A and B detect the fault. Circuit breaker A receives a restraint signal from B and remains closed for the full duration of its tripping delay set to 0.3. Circuit breaker B does not receive a signal from downstream and opens immediately, in spite of its tripping delay set to 0.2.

Limits to Device Interconnection:

  • A maximum of 15 upstreams devices may be connected to the ZSI input (Z1-Z2).

  • A maximum of 15 downstream devices may be connected to the ZSI input
    (Z3-Z4). If additional units are needed, a ZSI Interface Module is required.

ZSI Interface Module (ANSI 78)

The ZSI Interface Module in a ZSI system with MasterPacT MTZ circuit breakers equipped with MicroLogic X control units:

  • Boosts the voltage level of the restraint signal.

  • Converts the restraint signal to be compatible with other types of Schneider Electric™ circuit breakers (MasterPacT NT/NW) and Square D™ circuit breakers.

  • Provides double insulation to meet requirements of IEC standards when upstream and downstream are different generations of devices (MasterPacT MTZ, MasterPacT NT/NW).

Within a ZSI system, the voltage level of the restraint signal must be maintained at a certain level in order to activate the time delay of electronic trip devices.

If the restraint signal is too weak to activate the time delay feature, all devices that sense the fault will trip with no intentional delay.

The voltage level of the restraint signal can be ineffective due to:

  • Restraint wire length exceeding 300 m (984 ft.).

    If restraint wire length exceeds 300 m (984 ft.), the voltage drop along the control wire will weaken the restraint signal until it can no longer activate the time delay on the upstream device. If wire length exceeds 300 m (984 ft.), a ZSI module must be placed in the circuit to boost the voltage level of the restraint signal.

  • One device sending a restraint signal to many devices.

    In addition, if the number of upstream circuit breakers exceeds 15, then a ZSI module is required.

  • Varying signal levels from different electronic trip systems.

For further details on allowable ZSI combinations, please refer to the ZSI interface module installation bulletin NHA12883.

Characteristics

  • Maximum rated operational voltage (V): 690 Vac, 50/60 Hz.

  • Power supply: 24 Vdc +25/-20% , 6 mA.

  • Maximum operating temperature surrounding the module when installed inside electrical equipment: -35°C to 75°C (-31°F to 167°F).

  • Standards compliance: IEC 60950-1, CISPR 22, CISPR 24, UL 489, UL 489SE.

  • CE marked according to LVD (Low Voltage Directive 2014/35/EU) EN 60950-1 and EMC directive (2014/30/EU) EN55022, EN55024.

Connection & Installation

  • Terminal strips, jumpers and 35 mm DIN mounting rail (IEC/EN 60715).

  • Twisted wire with a braided shield, 300 Vac, 2.5–0.4 mm2 (22 AWG).

Instantaneous Override Protection and Close and Latch Ratings

The instantaneous override and close and latch are fixed trip settings to protect the circuit breaker when there is a high fault condition. These settings are typically higher than the standard instantaneous setting and function without regard to any other protection settings.

Instantaneous override is a fixed trip setting to open the circuit breaker, under 25 ms, in the event of fault which exceeds the instantaneous override trip value.

The close and latch rating is a fixed trip setting set lower than instantaneous override, to protect the circuit breaker in the event of closing the circuit breaker on an existing fault condition. After 20 ms the circuit breakers reverts to the "instantaneous override" setting.

MicroLogic X Control Unit Measurements

A MasterPacT MTZ device with embedded current sensors and MicroLogic X control unit is a power metering device complying with IEC/EN 61557-12, Class 0.5 accuracy for voltage and current and Class 1 accuracy for active power and energy measurements. For each measurement the accuracy is certified within a temperature range of -25 to 70°C (-13 to 158°F).

Measurements and Electrical Parameters Calculated by the Control Unit

Based on the measurement of line currents, neutral current, phase-to-phase voltages and phase-to-neutral voltages, a MicroLogic X control unit calculates* and displays parameters required to monitor any AC electrical power system:

  • RMS values of current and voltage

  • Active, reactive and apparent power

  • Active, reactive and apparent energy

  • Power factor

  • Frequency

  • Phase sequence

  • Voltage unbalance, current unbalance

  • Current demand

  • Total active, reactive and apparent power demand

  • THD of voltage and current

The calculation of current and power demand are performed in compliance with IEC/EN 61557-12.

Thermal Demand

Demand Calculated with a Sliding Block Interval

Electrical values calculated by MicroLogic X control units can be shown on the embedded HMI display, a smart device via Bluetooth, embedded web pages of Ethernet gateways, a PC running EcoStruxure Power Commission Software and on the FDM128 display unit. They are refreshed every 2 seconds. The display on the embedded HMI allows easy navigation through the electrical values and access to a Quickview option for the main basic values.

MicroLogic X control units log and time stamp minimum and maximum values since the last reset of all relevant measurements: currents, voltages, frequency, active power, reactive power, apparent power, total current harmonic distortion (THDI), total voltage harmonic distortion (THDV).... For the complete list of measurements and min / max values, see the MicroLogic X User Guide (DOCA0102EN). The maximum and minimum values are resettable from the embedded display, a smart device via Bluetooth technology or a PC running EcoStruxure Power Commission Software.

An optional external 24 Vdc power supply or the optional VPS module is required to process and display measurements below 20% of the rated current .

The phase-to-neutral voltages are available for four-pole and three-pole circuit breakers providing the connection of the VN terminal of MicroLogic X control units to the neutral. For accuracy of the active power measurement the connection of the VN terminal of MicroLogic X control units to the neutral is necessary. Please refer to the user guide (DOCA0102EN) for more details concerning the wiring and configuration of MicroLogic X control units.

Energy Management Functions of MicroLogic X Control Unit

Embedded sensors

A MasterPacT MTZ device equipped with a MicroLogic X control unit and its own embedded sensors is a Class 1 full chain measurement device for active power and energy metering*.

Embedded power metering avoids variation and uncertainty due to external sensors and wiring.

Effect of Temperature on MasterPacT MTZ Circuit Breaker Measurement

The effect of the temperature on accuracy of the measurement has been carefully managed to maintain an operating temperature between -13°F and 158°F (-25°C and 70°C).

MicroLogic X Control Unit Measurement Values

Type of Measurement

Symbol

Accuracy

Range Min. Acc

Range Max. Acc

Unit

EHMI *

FDM 128

EcoStruxure Power Commission Software,
EIFE, IFE, IFM

Currents

RMS Current of Phases

I1, I2, I3, Iavg

±0.5%

40 *

4,000 x 1.2 *

A

RMS Current of Phases

I1, I2, I3, Iavg

±0.5%

40 *

4,000 x 1.2 *

A

Voltages

RMS Phase-to-Phase Voltage

V12, V23, V31,
VLL average

±0.5%

208

690 x 1.2

V

RMS Phase-to-Neutral Voltage

V1N, V2N, V3N, VLN average *

±0.5%

120

400 x 1.2

V

Power and Energy

Active Power

P1, P2, P3, Ptot

±1 %

5

10,000

(±) kW

Reactive Power

Q1, Q2, Q3, Qtot

±2%

5

10,000

(±) kVAR

Apparent Power

S1, S2, S3, Stot

±1%

5

10,000

kVA

Power Factor

PF

±0.02

-1

1

 

Power Factor / Phase

PF1, PF2, PF3

±0.02

-1

1

 

Fundamental Power Factor (cos φ or DPF)

Cos φ

±0.02

-1

1

 

Fundamental Power Factor (cos φ or DPF) / Phase

Cos φ1, Cos φ2, Cos φ3

±0.02

-1

1

 

Active Energy *

Ep IN / OUT / total *

±1%

0

10,000,000

kWh

Reactive Energy *

Eq IN / OUT / total *

±2%

0

10,000,000

kVARh

Apparent Energy *

Es IN / OUT / total *

±1%

0

10,000,000

kVAh

Active Energy *

Ep IN / OUT / total *

±1%

0

10,000,000

kWh

Reactive Energy *

Eq IN / OUT / total *

±2%

0

10,000,000

kVARh

Apparent Energy *

Es IN / OUT / total *

±1%

0

10,000,000

kVAh

Current and Power Demands

Current demands

I1, I2, I3, IN, Iavg

±0.5%

40 *

4,000 x 1.2 *

A

Total active power demand

Ptot

±1%

5

10,000

(±) kW

Total reactive power demand

Qtot

±2%

5

10,000

(±) kVAR

Total apparent power demand

Stot

±1%

5

10,000

kVA

Power Quality

Frequency

F

±0.005

40

70

Hz

Phase Sequence
(0: a,b,c /1,2,3 - 1: a,c,b /
1,3,2)

Phase sequence

NA

1 2 3

1 3 2

0 - 1

RMS Current on Neutral

IN

Neutral current available only with four-pole circuit breakers or three-pole circuit breakers with External Neutral Current Transformer (ENCT).

*

±1%

40 *

4,000 *

A

RMS Current on Ground Current

Ig

±5%

40 *

4,000 *

A

THDI Current Phase

ITHD I1, I2, I3, Iavg

Cl 5 *

0 %

100 % *

% *

*

THDI I Neutral

ITHD IN

Neutral current available only with four-pole circuit breakers or three-pole circuit breakers with External Neutral Current Transformer (ENCT).

*

Cl 5 *

0%

100% *

%*

*

THDU Phase-to-Phase voltage

VTHD V12,23,31, LLavg

Cl 2 *

0%

20% *

%*

*

THDV Phase-N Voltages

VTHD V1N,2N,3N, LNavg *

Cl 2 *

0%

20% *

%*

*

Current Unbalance vs Average 3 Phase RMS Currents

I_unbal 1,2,3, Iunbal (worst)

+5%

0%

100%

%

Phase-to-Phase Voltage Unbalance

VLL_Unbal 12 23 31 unbal

Cl 0.5

0%

10%

%

Phase-to-Neutral Voltage Unbalance

VLN_Unbal 1N, 2N 3N, unbal*

Cl 0.5

0%

10%

%

NOTE: MicroLogic X control units log and time stamp minimum and maximum values since last reset of all relevant measurements. Main maximum values may be read on embedded HMI (Currents, Voltages, Frequence, Ptotal, Qtotal, THDIavg, THDUavg,THDIN ...). For a complete list of measurements and min. / max. values, see the MicroLogic X User Guide DOCA0102EN.

MicroLogic X Control Unit Diagnostics and Maintenance

The MicroLogic X control unit performs a high level of diagnostics in real time on MasterPacT MTZ circuit breakers. They generate and store appropriate warnings, alarms, and messages to help the users with maintenance and power restoration.

These diagnostics:

  • Prevent interruption of the power supply to maintain continuity of operation, preserve assets from damage, and support the safety of personnel.

  • Reduce downtime resulting from an unexpected outage in the electrical distribution system by facilitating a restart as quickly as possible after a trip.

  • Keep devices in good operating condition and aid qualified personnel when repairs are required.

  • Build the history and traceability of all interventions to improve preventive maintenance and secure daily operation.

Prevention of Power Supply Interruptions

The MicroLogic X control unit monitors the condition of the circuit breaker and generates information to help in scheduling periodic checks and, if needed, replacement of devices.

Most of the active mechanical and electrical components of the circuit breaker and the control unit are monitored. Warnings and alarms are issued when issues requiring the intervention of the maintenance staff are detected.

Maintenance recommendations are based on monitoring the operation and performance of the circuit breaker (such as number of operations, closing, and opening times). When threshold limits are reached or exceeded, alarms and warnings are issued to advise operators to plan maintenance.

The MicroLogic X control unit monitors parameters to estimate circuit breaker aging (load profile, contact wear, and the end of life indicator for instance). Based on the these values, algorithms identify if maintenance or part replacement is needed.

NOTE: for further details please refer to Power Shutdown Prevention and Repair and MasterPacT MTZ Services.

Restart After a Trip

The LEDs on the front of the MicroLogic X control unit identify the tripping cause. Relevant information characterizing the fault can be retrieved using a smart phone or device via either Bluetooth technology or NFC or using EcoStruxure Power Commission Software on a PC.

Warning and Alarm Displays

The MicroLogic X control unit has a "Service" LED to indicate the circuit breaker condition. This LED, represented by a "wrench / spanner", has three states:

  • Unlit LED: the unit is in good working order.

  • Orange LED: non-urgent intervention is required (contact wear above 60% for example).

  • Red LED: alert message that requires immediate intervention (such as contact wear above 100% or an invalid control unit self test).

The messages processed by the MicroLogic X control unit to monitor circuit breaker availability and maintenance operations are classified in three categories:

  • Maintenance assistance

  • Circuit breaker condition

  • Circuit breaker diagnostics

The associated warnings and alarms are displayed on the embedded HMI. The warnings are displayed with an orange backlight, the alarm with a red backlight.

When the MicroLogic X control unit is not energized only the trip alarms with their associated messages remain accessible with a smart phone through NFC.

The various possibilities to display warnings, alarms and messages concerning the management of maintenance and the condition of the circuit breaker are summarized in the following table:

 

Trip Unit Energized

Trip Unit Not Energized

 

Display on embedded HMI Warning

Display on embedded HMI Alarm

Display on smart phone with Bluetooth technology

EcoStruxure Power Commission Software USB connection

Display On FDM128

IFE/EIFE web pages

Display trip alarm on smartphone with NFC

Warnings

Orange Backlight

Alarms

Red Backlight

Prevent Power Shutdown with Conditional Checks

Monitored Functions and Logs for Circuit Breaker Operation

Elect. Closing Function

Elect. Opening Function

Tripping Function

  • XF coil circuit continuity

  • MCH charging time

  • “Time stamped” closing log

  • MCH counter

  • Alarm fail closing order

  • MX coil circuit continuity

  • MN coil circuit continuity

  • Opening counter

  • “Time stamped” opening log (Electrical/ mechanical)

  • Alarm fail opening order

  • Tripping chain continuity (Ready LED)

  • Trip counter (SDE)

  • Time stamped event log

Monitored Functions & Logs Fault Detection on MicroLogic X

External Sensors Disconnection

MicroLogic X Control Unit Problem

External Communication Problem

  • Internal Current Transformers [T]

  • External Neutral CT

  • Vigi Sensor

  • ASIC over temp [T]

  • ASIC problem [T]

  • Error reading perform / Sensor rating

  • Internal battery

  • Trip solenoid is not connected, default is to trip the circuit breaker

  • Bluetooth error

  • Ethernet Error communication (IFE)

  • IO module

Repairing a Device

The MicroLogic X control unit includes dedicated functions for maintenance assistance.

The following information can be retrieved:

  • Serial number and features of the circuit breaker.

  • Optional accessories installed on the circuit breaker.

  • References for spare parts and replacement accessories.

  • Type of problem encountered with maintenance assistance information.

MicroLogic X Control Unit Event Management

Event History

Number of Events

Trip

50

Protection

100

Diagnostic

300

Metering

300

Configuration

100

Operation

300

Communication

100

A list of predefined events has been selected for user notification of alarms and traceability processed by a MicroLogic X control unit.

These events are classified in seven families: trip, protection, diagnostic, metering, configuration, operation, and communication.

Definition and Categories of Events

MicroLogic X control unit functions produce events available for alarm notification or history logging, in addition to their main action of tripping, measuring, and counting.

All events are time stamped and logged in non-volatile memory so they are maintained if control power is lost.

Events have two characteristics:

  • Event category: trip, protection, diagnostic, metering, configuration, operation, communication

  • Event severity: high-level, medium-level, low-level

Events can be of two types:

  • occurrence/completion

  • instantaneous/latched/unlatched

Event Logbooks

Events are logged according to the event category:

  • Trip: long-time trip, short-time trip, trip on invalid control unit self test...

  • Protection: setting change, I > 90% Ir long time, change from set A to set B ...

  • Diagnostic: voltage release, low battery ...

  • Metering: reset min. / max., reset energy counters…

  • Configuration: digital module license …

  • Operation: opening, closing, alarm reset...

  • Communication: Bluetooth enabled ...

All events are logged regardless of their severity. Each history can log a predefined number of events. When that number is reached each new event overwrites the oldest event, and other histories are left unchanged (first-in first-out [FIFO]).

For the complete list of events see the MicroLogic X control unit user guide DOCA0102EN.

Event Notification

  • High severity events generate pop-ups on embedded HMI with a red backlight.

  • Medium severity events generate pop-ups on embedded HMI with an orange backlight.

  • On the FDM128 display unit they change the related pictogram color to red for high severity events or orange for medium severity events.

  • All events can be signalled individually or by group to a digital output (M2C or IO module).

  • All events can trigger an email through EIFE or IFE communication interfaces.

  • High and medium severity events can be read on the embedded HMI, a PC or a smart phone.

  • All the events logged can be displayed with EcoStruxure Power Commission Software, a smart phone or the FDM128 display. They are shown in chronological order. They can be sorted according to the following selections: date and time, severity, or category.

Event Type and Reset Mode

There are two types of events:

Occurrence / Completion events: These events have a beginning and an end (for example: long-time pick-up and dropout).

Instantaneous events: These events have no duration (for example reception of an opening order, circuit breaker tripping or settings changes).

An event may be latched or unlatched:

  • A latched event does not reset automatically. It remains in hold position after its cause has disappeared or until it is reset by the user.

  • An unlatched event is active while its cause is present and returns to inactive as soon as its cause disappears or is resolved.

For latched events a reset action can be made:

  • From the test/reset button on the front face of the MicroLogic control unit.

  • From a PC.

  • From a smart phone.

  • Via Ethernet and Modbus SL (RTU) through the EIFE, IFE and IFM interfaces.

Use a PC, a smartphone, Ethernet or Modbus SL (RTU) to reset events managed by the MicroLogic X control unit.

MicroLogic X Control Unit Power Supply

The MicroLogic X control unit is powered by the current through the internal current transformers (CT).

The standard protection functions of MicroLogic X control units operate with the internal current supply.

Internal Power Supplies

If the load current is higher than 20% of the rated current In, the internal current supply provides the power supply for the full functioning of the MicroLogic X control unit. This includes:

  • The MicroLogic X HMI, display screen, and LEDs.

  • The metering functions with accuracies in accordance with IEC 61557-12.

  • The maintenance and diagnostic functions.

  • Communication through ULP modules.

  • Communication through Bluetooth low energy technology.

External Power Supplies

To provide a power supply to the MicroLogic X control unit when the load is below 20% of the rated current In, and maintain the full functioning of the MicroLogic X control unit, optional power supplies can be used. Optional power supplies include the following:

  • Permanent power supplies:

    • Internal voltage power supply (VPS) module, up to 600 Vac.

    • External 24 Vdc power supply.

  • Temporary power supplies connected to the mini USB port of the MicroLogic X control unit:

    • External Mobile Power Pack through USB connection.

    • Android smartphone through USB OTG connection (smartphone must be compatible with USB OTG - see list of compatible smartphones available on the Schneider Electric website).

    • PC through USB connection.

MicroLogic X control units are also equipped with an internal battery dedicated to the supply of the LED indicators and the internal clock. It allows the user to read and identify the trip cause when the circuit breaker trips. This is a Lithium type battery, to check the battery condition, press the test button on the front of the MicroLogic X control unit.

An external 24 Vdc power supply is required when IFE/EIFE/IFM communication modules, IO modules or an FDM128 display unit are installed.

The XF diag&com, MX diag&com, MN diag, XF, MX, and MN voltage release coils and the spring charging motor MCH require a power supply separate from the MicroLogic X control unit power supply.

MicroLogic X Control Unit Voltage Measurement Inputs

The input voltage of the VPS module is limited to 600 Vac. The module is directly connected to the internal pickup voltage (PTI) on the downstream side of the circuit breaker. The VPS module can be supplied from an external voltage by means of the optional PTE voltage measurement inputs and voltage transformers (mandatory for voltages above 600 Vac).

The external voltage can be picked up either from the top or the bottom side of the circuit breaker.

When the power source and the PTE option are connected on the same side of the circuit breaker (for example, both the power source and the PTE are connected on the top side), the MicroLogic X control unit is energized as soon as the power source is live, whatever the position of the circuit breaker (open or closed).

When the power source and the PTE option are connected on different sides of the circuit breaker (for example, the power source is connected on the top side and the PTE on the bottom side), the MicroLogic X control unit is energized only when the circuit breaker is closed.

The possible VT ratio are the following:

  • Primary range:

    • Min value: 100 V

    • Max value: 1250 V

  • Secondary range:

    • Min value: 100 V

    • Max value: 690 V

    • Recommended values: 220-400 V

  • Power ≥ 10 VA

  • Max voltage for VPS is 600 V (see Voltage Power Supply Module (VPS))

Recommended Alternative Power Sources

Recommended Alternative Power Sources in Different Situations

Situation

Purpose

VPS

External 24 Vdc Power Supply

PC Supply

Portable Battery

Circuit breaker is energized and current is < 20% of rated current.

Maintains protection functions, measurement data, communication, diagnostic data, HMI, and wireless features.

Circuit breaker is opened or not energized.

Retrieve information from control unit front screen/embedded HMI or with Bluetooth connection.

During setting, commissioning, testing and maintenance.

Complete any testing or evaluation of the breaker function or control devices.

When IFE/EIFE, IO module or FDM128 is installed.

These devices require a power supply.

NOTE: For more information about the VPS module, the external 24 Vdc supply, and the portable battery, please refer to MasterPacT MTZ Power Supply Accessories.
 

MicroLogic X

EIFE

IFE

IO Module

FDM128

Without M2C

With M2C

Power consumption (mA) 24 Vdc

250

300

250

150

150

283

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.